<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Script to Unlock JTAG via Trace32</title>
    <link>https://community.nxp.com/t5/S32K/Script-to-Unlock-JTAG-via-Trace32/m-p/2171051#M52768</link>
    <description>Thanks, I will check and let you know &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;</description>
    <pubDate>Wed, 17 Sep 2025 10:07:58 GMT</pubDate>
    <dc:creator>NileshDharap</dc:creator>
    <dc:date>2025-09-17T10:07:58Z</dc:date>
    <item>
      <title>Script to Unlock JTAG via Trace32</title>
      <link>https://community.nxp.com/t5/S32K/Script-to-Unlock-JTAG-via-Trace32/m-p/2170439#M52717</link>
      <description>&lt;P&gt;Hello Team,&lt;BR /&gt;&lt;BR /&gt;I am working on S32K3x controller. I will be locking the JTAG using HSE with a key.&lt;BR /&gt;&lt;BR /&gt;I am looking for a script which will do the following things when I connect to Trace32&lt;BR /&gt;&lt;BR /&gt;1. The script checks if Debug interface is locked.&lt;BR /&gt;2. If yes, read PW from password.txt (some file).&lt;BR /&gt;3. Attach command to unlock JTAG.&lt;BR /&gt;&lt;BR /&gt;I saw almost all the queries here, either it uses some external application or accesses JTAG Port directly to unlock it (S32_JTAG_WRITE.cmm). I am not sure whether it works when JTAG is locked via HSE. I suspect it doesn't.&amp;nbsp;&lt;BR /&gt;I haven't tried any since I don't want to brick by controller.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Can someone help here please, I'll provide any other info if needed.&lt;BR /&gt;&lt;BR /&gt;Thanks in advance.&lt;BR /&gt;Nilesh&lt;/P&gt;</description>
      <pubDate>Tue, 16 Sep 2025 12:00:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Script-to-Unlock-JTAG-via-Trace32/m-p/2170439#M52717</guid>
      <dc:creator>NileshDharap</dc:creator>
      <dc:date>2025-09-16T12:00:44Z</dc:date>
    </item>
    <item>
      <title>Re: Script to Unlock JTAG via Trace32</title>
      <link>https://community.nxp.com/t5/S32K/Script-to-Unlock-JTAG-via-Trace32/m-p/2170440#M52718</link>
      <description>Also, I used to perform Unlocking with the below command for MPC5476C controller&lt;BR /&gt;&lt;BR /&gt;sys.option.KEYCODE 0x11111111 0x22222222 0x33333333 0x44444444 0x55555555 0x66666666 0x77777777 0x88888888.&lt;BR /&gt;&lt;BR /&gt;Will it work the same as for S32K3 as well? That would be also helpful to know</description>
      <pubDate>Tue, 16 Sep 2025 12:04:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Script-to-Unlock-JTAG-via-Trace32/m-p/2170440#M52718</guid>
      <dc:creator>NileshDharap</dc:creator>
      <dc:date>2025-09-16T12:04:28Z</dc:date>
    </item>
    <item>
      <title>Re: Script to Unlock JTAG via Trace32</title>
      <link>https://community.nxp.com/t5/S32K/Script-to-Unlock-JTAG-via-Trace32/m-p/2170968#M52765</link>
      <description>&lt;P&gt;No, as I know it cannot be used this simple way.&lt;/P&gt;
&lt;P&gt;I have recently tested it with scripts I am attaching.&lt;/P&gt;
&lt;P&gt;Hope it helps&lt;/P&gt;</description>
      <pubDate>Wed, 17 Sep 2025 08:31:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Script-to-Unlock-JTAG-via-Trace32/m-p/2170968#M52765</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2025-09-17T08:31:12Z</dc:date>
    </item>
    <item>
      <title>Re: Script to Unlock JTAG via Trace32</title>
      <link>https://community.nxp.com/t5/S32K/Script-to-Unlock-JTAG-via-Trace32/m-p/2171051#M52768</link>
      <description>Thanks, I will check and let you know &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;</description>
      <pubDate>Wed, 17 Sep 2025 10:07:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Script-to-Unlock-JTAG-via-Trace32/m-p/2171051#M52768</guid>
      <dc:creator>NileshDharap</dc:creator>
      <dc:date>2025-09-17T10:07:58Z</dc:date>
    </item>
  </channel>
</rss>