<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Missing TCP/IP stack in example project in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Missing-TCP-IP-stack-in-example-project/m-p/2166495#M52559</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I am working with S32K1 series boards, S32K148 more concretely.&lt;/P&gt;
&lt;P&gt;The issue I face is that not even the example project compiles. I create it using S32DS IDE and "New -&amp;gt; Project from Example", from which I select the lwip_FreeRTOS_S32K148.&lt;/P&gt;
&lt;P&gt;The documentation says it should be possible to build it straight from there. However, that is not the case because a lot of files are missing. After opening the S32 Configuration Tools and Updating the Code, most of the issues are gone. However, the lwip stacks folder is still missing and I get an error in the Peripherals tab saying that the tcp/ip stack is not included in the toolchain.&lt;/P&gt;
&lt;P&gt;As stated in the Release Notes of the stack, I installed&amp;nbsp;S32K1_S32M24X Real Time Drivers AUTOSAR R21-11 Version 3.0.0 and S32K1 FreeRTOS 10.5.1&lt;BR /&gt;version 2.0.0 packages and I am using S32DS 3.6.3.&lt;/P&gt;</description>
    <pubDate>Wed, 10 Sep 2025 09:00:48 GMT</pubDate>
    <dc:creator>sergioGeronimo</dc:creator>
    <dc:date>2025-09-10T09:00:48Z</dc:date>
    <item>
      <title>Missing TCP/IP stack in example project</title>
      <link>https://community.nxp.com/t5/S32K/Missing-TCP-IP-stack-in-example-project/m-p/2166495#M52559</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I am working with S32K1 series boards, S32K148 more concretely.&lt;/P&gt;
&lt;P&gt;The issue I face is that not even the example project compiles. I create it using S32DS IDE and "New -&amp;gt; Project from Example", from which I select the lwip_FreeRTOS_S32K148.&lt;/P&gt;
&lt;P&gt;The documentation says it should be possible to build it straight from there. However, that is not the case because a lot of files are missing. After opening the S32 Configuration Tools and Updating the Code, most of the issues are gone. However, the lwip stacks folder is still missing and I get an error in the Peripherals tab saying that the tcp/ip stack is not included in the toolchain.&lt;/P&gt;
&lt;P&gt;As stated in the Release Notes of the stack, I installed&amp;nbsp;S32K1_S32M24X Real Time Drivers AUTOSAR R21-11 Version 3.0.0 and S32K1 FreeRTOS 10.5.1&lt;BR /&gt;version 2.0.0 packages and I am using S32DS 3.6.3.&lt;/P&gt;</description>
      <pubDate>Wed, 10 Sep 2025 09:00:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Missing-TCP-IP-stack-in-example-project/m-p/2166495#M52559</guid>
      <dc:creator>sergioGeronimo</dc:creator>
      <dc:date>2025-09-10T09:00:48Z</dc:date>
    </item>
    <item>
      <title>Re: Missing TCP/IP stack in example project</title>
      <link>https://community.nxp.com/t5/S32K/Missing-TCP-IP-stack-in-example-project/m-p/2166566#M52562</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254540"&gt;@sergioGeronimo&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;This is caused by a mismatch in manifest SDK version between RTD 3.0.0 (&lt;STRONG&gt;version 2.0.0&lt;/STRONG&gt;) and TCP/IP 3.0.0 (&lt;STRONG&gt;version 3.0.0&lt;/STRONG&gt;) releases.&lt;/P&gt;
&lt;P&gt;To solve this please follow these steps:&lt;/P&gt;
&lt;P&gt;1. Go in S32DS installation folder, or the equivalent path for your machine.&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;C:\NXP\S32DS.3.6.1\S32DS\software\PlatformSDK_S32K1_S32M24&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;2. Open the&amp;nbsp;&lt;STRONG&gt;tcpip_itm_manifest.xml&amp;nbsp;&lt;/STRONG&gt;and change the version from 3.0.0 to 2.0.0&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PavelL_0-1757499391080.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356233i7695E3290C4ECA2E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PavelL_0-1757499391080.png" alt="PavelL_0-1757499391080.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;3. Restart S32DS&lt;/P&gt;
&lt;P&gt;4. Open peripheral view and run "Update Code"&lt;/P&gt;
&lt;P&gt;5. run Build again&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 10 Sep 2025 10:17:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Missing-TCP-IP-stack-in-example-project/m-p/2166566#M52562</guid>
      <dc:creator>PavelL</dc:creator>
      <dc:date>2025-09-10T10:17:20Z</dc:date>
    </item>
  </channel>
</rss>