<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32k144 VDD/VDDA</title>
    <link>https://community.nxp.com/t5/S32K/S32k144-VDD-VDDA/m-p/951306#M5242</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Can I put:&lt;/P&gt;&lt;P&gt;VDD1,VDD2,VDD3,VDD4 in 3V3&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;VDDA,VREFH in 5V?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Aug 2019 18:25:31 GMT</pubDate>
    <dc:creator>lohrsistemas</dc:creator>
    <dc:date>2019-08-05T18:25:31Z</dc:date>
    <item>
      <title>S32k144 VDD/VDDA</title>
      <link>https://community.nxp.com/t5/S32K/S32k144-VDD-VDDA/m-p/951306#M5242</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Can I put:&lt;/P&gt;&lt;P&gt;VDD1,VDD2,VDD3,VDD4 in 3V3&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;VDDA,VREFH in 5V?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Aug 2019 18:25:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k144-VDD-VDDA/m-p/951306#M5242</guid>
      <dc:creator>lohrsistemas</dc:creator>
      <dc:date>2019-08-05T18:25:31Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 VDD/VDDA</title>
      <link>https://community.nxp.com/t5/S32K/S32k144-VDD-VDDA/m-p/951307#M5243</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Is not possible to achieve what you mentioned. VDD1, VDD2, VDD3, VDD4, and VDDA must be shorted to a common source on PCB. And VREFH should always be equal to or less than VDDA + 0.1 V and VDD + 0.1 V.&lt;/P&gt;&lt;P&gt;So, all VDDx voltages should be equal and if VDDx is 3.3V, VREFH must not exceed 3.4V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Aug 2019 21:19:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k144-VDD-VDDA/m-p/951307#M5243</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2019-08-06T21:19:15Z</dc:date>
    </item>
  </channel>
</rss>