<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K344-WB Port Pin Configuration</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-WB-Port-Pin-Configuration/m-p/2162421#M52338</link>
    <description>&lt;P&gt;I have a few questions on configuring pins for my S32K344-WB board.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN&gt;For the&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Siul2_port&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;I could use some help configuring it. Looking at the Siul2_port/PortConfigSet tab, do I need to add an entry for every pin on the MCU being used? I have a total of 78 pins being used, of which 46 pins are SIUL2 type.&lt;/SPAN&gt;&lt;/LI&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN&gt;if not, what goes on PortConfigSet tab?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;if so, how do I go about adding the pins and configuring them?&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;/OL&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN&gt;Each pin also relates to a LLR driver. I have configured the LPSPI driver tab. Do I need to add a driver component for each type on the Pins tab? In other words, I have pins in each of these types, ADC, WKPU, System, JTAG. Do I need to add the corresponding LLR Driver component for each one?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;When adding LLR Components from "Add Configuration Component Instance" window, not all components seem to be available. Some have a yellow triangle and a note that "they are not found in the tool chain" How do I resolve that ?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Which Peripherals Component do I add to configure interrupts and ISRs using the LLRs. in the MCAL I think it would be the platform component, but I don't see an equivalent in the LLR Add menu.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;</description>
    <pubDate>Tue, 02 Sep 2025 23:02:05 GMT</pubDate>
    <dc:creator>ekmas-19</dc:creator>
    <dc:date>2025-09-02T23:02:05Z</dc:date>
    <item>
      <title>S32K344-WB Port Pin Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-WB-Port-Pin-Configuration/m-p/2162421#M52338</link>
      <description>&lt;P&gt;I have a few questions on configuring pins for my S32K344-WB board.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN&gt;For the&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Siul2_port&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;I could use some help configuring it. Looking at the Siul2_port/PortConfigSet tab, do I need to add an entry for every pin on the MCU being used? I have a total of 78 pins being used, of which 46 pins are SIUL2 type.&lt;/SPAN&gt;&lt;/LI&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN&gt;if not, what goes on PortConfigSet tab?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;if so, how do I go about adding the pins and configuring them?&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;/OL&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN&gt;Each pin also relates to a LLR driver. I have configured the LPSPI driver tab. Do I need to add a driver component for each type on the Pins tab? In other words, I have pins in each of these types, ADC, WKPU, System, JTAG. Do I need to add the corresponding LLR Driver component for each one?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;When adding LLR Components from "Add Configuration Component Instance" window, not all components seem to be available. Some have a yellow triangle and a note that "they are not found in the tool chain" How do I resolve that ?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Which Peripherals Component do I add to configure interrupts and ISRs using the LLRs. in the MCAL I think it would be the platform component, but I don't see an equivalent in the LLR Add menu.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;</description>
      <pubDate>Tue, 02 Sep 2025 23:02:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-WB-Port-Pin-Configuration/m-p/2162421#M52338</guid>
      <dc:creator>ekmas-19</dc:creator>
      <dc:date>2025-09-02T23:02:05Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344-WB Port Pin Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-WB-Port-Pin-Configuration/m-p/2165347#M52507</link>
      <description>&lt;P&gt;Thank you for your interest in our products and for contributing to our community.&lt;BR /&gt;&lt;BR /&gt;1. You should fill the &lt;EM&gt;PortPin Mscr&lt;/EM&gt; value for each pin you have configured in &lt;EM&gt;Pins Tool&lt;/EM&gt;. Since RTD 6.0.0 this step is not necessary. it fills automatically.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="_Leo__0-1757352713857.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/355954i9D40B169BEFDCCD4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="_Leo__0-1757352713857.png" alt="_Leo__0-1757352713857.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;2. Regardless of the peripheral configuration in &lt;EM&gt;Peripherals Tool&lt;/EM&gt;. If such signal are routed to an external pad, then it is needed its respective configuration in &lt;EM&gt;Pins Tool&lt;/EM&gt;.&lt;BR /&gt;3. You just add them, &lt;EM&gt;Update Code&lt;/EM&gt; and write in main file its respective include.&lt;BR /&gt;4. For interrupt configuration use the &lt;EM&gt;IntCtrl_Ip&lt;/EM&gt; driver.&lt;BR /&gt;&lt;BR /&gt;I hope this information is helpful.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Sep 2025 17:34:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-WB-Port-Pin-Configuration/m-p/2165347#M52507</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2025-09-08T17:34:21Z</dc:date>
    </item>
  </channel>
</rss>