<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32k328 flashing in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32k328-flashing/m-p/2162177#M52333</link>
    <description>&lt;P&gt;HI everyone,&lt;/P&gt;&lt;P&gt;we have one hardware, and there is already one image is present, and we are trying to flash the base image(empty image with for loop) which is created by Design studio.&lt;/P&gt;&lt;P&gt;we can't use design studio to flash, we have one flashing script which is verified, after we flash the very basic image , we can't flash again the any image even the older image, we are getting some error on gdb , could any explain me what is happing here, and to solve this&lt;/P&gt;&lt;P&gt;Error: Failed to read memory at 0xe000ed00&lt;BR /&gt;Examination failed, GDB will be halted. Polling again in 700ms&lt;BR /&gt;Warn : VECTRESET is not supported on your Cortex-M core!&lt;BR /&gt;requesting target halt and executing a soft reset&lt;BR /&gt;Info : SWD DPIDR 0x6ba02477&lt;BR /&gt;target halted due to breakpoint, current mode: Thread&lt;BR /&gt;xPSR: 0x01000000 pc: 0x00402420 msp: 0x20010000&lt;BR /&gt;Polling target s32k3xx.armv7m.cm7_0 failed, trying to reexamine&lt;BR /&gt;Info : s32k3xx.armv7m.cm7_0: hardware has 8 breakpoints, 4 watchpoints&lt;BR /&gt;target halted due to debug-request, current mode: Thread&lt;BR /&gt;xPSR: 0x61000000 pc: 0x00402624 msp: 0x20010000&lt;BR /&gt;target halted due to debug-request, current mode: Handler HardFault&lt;BR /&gt;xPSR: 0x01000003 pc: 0x004026a6 msp: 0x2000ffe0&lt;BR /&gt;Error: s32k3xx.armv7m.cm7_0 -- clearing lockup after double fault&lt;BR /&gt;target halted due to debug-request, current mode: Handler HardFault&lt;BR /&gt;xPSR: 0x01000003 pc: 0x204084e4 msp: 0x2000ffe0Polling target s32k3xx.armv7m.cm7_0 failed, trying to reexamine&lt;BR /&gt;Info : s32k3xx.armv7m.cm7_0: hardware has 8 breakpoints, 4 watchpoints&lt;BR /&gt;shutdown command invoked&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 02 Sep 2025 13:00:38 GMT</pubDate>
    <dc:creator>leo_Z</dc:creator>
    <dc:date>2025-09-02T13:00:38Z</dc:date>
    <item>
      <title>S32k328 flashing</title>
      <link>https://community.nxp.com/t5/S32K/S32k328-flashing/m-p/2162177#M52333</link>
      <description>&lt;P&gt;HI everyone,&lt;/P&gt;&lt;P&gt;we have one hardware, and there is already one image is present, and we are trying to flash the base image(empty image with for loop) which is created by Design studio.&lt;/P&gt;&lt;P&gt;we can't use design studio to flash, we have one flashing script which is verified, after we flash the very basic image , we can't flash again the any image even the older image, we are getting some error on gdb , could any explain me what is happing here, and to solve this&lt;/P&gt;&lt;P&gt;Error: Failed to read memory at 0xe000ed00&lt;BR /&gt;Examination failed, GDB will be halted. Polling again in 700ms&lt;BR /&gt;Warn : VECTRESET is not supported on your Cortex-M core!&lt;BR /&gt;requesting target halt and executing a soft reset&lt;BR /&gt;Info : SWD DPIDR 0x6ba02477&lt;BR /&gt;target halted due to breakpoint, current mode: Thread&lt;BR /&gt;xPSR: 0x01000000 pc: 0x00402420 msp: 0x20010000&lt;BR /&gt;Polling target s32k3xx.armv7m.cm7_0 failed, trying to reexamine&lt;BR /&gt;Info : s32k3xx.armv7m.cm7_0: hardware has 8 breakpoints, 4 watchpoints&lt;BR /&gt;target halted due to debug-request, current mode: Thread&lt;BR /&gt;xPSR: 0x61000000 pc: 0x00402624 msp: 0x20010000&lt;BR /&gt;target halted due to debug-request, current mode: Handler HardFault&lt;BR /&gt;xPSR: 0x01000003 pc: 0x004026a6 msp: 0x2000ffe0&lt;BR /&gt;Error: s32k3xx.armv7m.cm7_0 -- clearing lockup after double fault&lt;BR /&gt;target halted due to debug-request, current mode: Handler HardFault&lt;BR /&gt;xPSR: 0x01000003 pc: 0x204084e4 msp: 0x2000ffe0Polling target s32k3xx.armv7m.cm7_0 failed, trying to reexamine&lt;BR /&gt;Info : s32k3xx.armv7m.cm7_0: hardware has 8 breakpoints, 4 watchpoints&lt;BR /&gt;shutdown command invoked&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Sep 2025 13:00:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k328-flashing/m-p/2162177#M52333</guid>
      <dc:creator>leo_Z</dc:creator>
      <dc:date>2025-09-02T13:00:38Z</dc:date>
    </item>
    <item>
      <title>Re: S32k328 flashing</title>
      <link>https://community.nxp.com/t5/S32K/S32k328-flashing/m-p/2162849#M52371</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252204"&gt;@leo_Z&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;From the short log I see the debugger reports that the application core detected a fault exception.&lt;/P&gt;
&lt;P&gt;Do you have any other debuggers?&lt;/P&gt;
&lt;P&gt;Have you tried both SWD and JTAG protocols?&lt;/P&gt;
&lt;P&gt;Can you just attach the debugger to the MCU without programming it?&lt;/P&gt;
&lt;P&gt;Can you debug the code right from the reset handler?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Try keeing the MCU in reset as described here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-SDK/failed-to-power-up-dap-after-program-s32k312-with-pll0-equal/td-p/1609010" target="_blank"&gt;https://community.nxp.com/t5/S32-SDK/failed-to-power-up-dap-after-program-s32k312-with-pll0-equal/td-p/1609010&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 03 Sep 2025 11:05:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k328-flashing/m-p/2162849#M52371</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-09-03T11:05:05Z</dc:date>
    </item>
  </channel>
</rss>