<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K3xx SAR ADC resolution in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K3xx-SAR-ADC-resolution/m-p/2160385#M52253</link>
    <description>&lt;P&gt;Hi&amp;nbsp;Sean,&lt;/P&gt;
&lt;P&gt;Section &lt;STRONG&gt;60.2.2 Features&lt;/STRONG&gt; of the &lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K3XXRM" target="_self"&gt;S32K3XXRM&lt;/A&gt; states:&lt;BR /&gt;&lt;FONT color="#808080"&gt;•Selectable resolution (8-, 10-, 12-, &lt;STRONG&gt;14-bit&lt;/STRONG&gt;). Note that the conversion result is always 15 bits wide, even if the selected resolution is smaller (see CALBISTREG[RESN]).&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#808080"&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="60.2.2 Features Selectable resolution (8-, 10-, 12-, 14-bit).png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/354701iD320048C220B6B0C/image-size/large?v=v2&amp;amp;px=999" role="button" title="60.2.2 Features Selectable resolution (8-, 10-, 12-, 14-bit).png" alt="60.2.2 Features Selectable resolution (8-, 10-, 12-, 14-bit).png" /&gt;&lt;/span&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P data-unlink="true"&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/S32K3xx.pdf" target="_self"&gt;S32K3&amp;nbsp;DataSheet&lt;/A&gt;&amp;nbsp;states: TUE spec for precision and standard channels is based on 12-bit level resolution.&lt;BR /&gt;If you set the resolution to 14-bit, the TUE is only slightly better than that of 12-bit resolution.&lt;/P&gt;
&lt;P data-unlink="true"&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Fri, 29 Aug 2025 05:59:40 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2025-08-29T05:59:40Z</dc:date>
    <item>
      <title>S32K3xx SAR ADC resolution</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-SAR-ADC-resolution/m-p/2160239#M52244</link>
      <description>&lt;P&gt;Dear sir,&lt;/P&gt;&lt;P&gt;I see S32K3xx SAR ADC supports max 12bit resolution in spec.&lt;/P&gt;&lt;P&gt;But the conversion resolution in example code from RTD is 14 bit(Adc_Sar_Bctu_Ip_example_S32K344, SAdc_Sar_Bctu_Ip_example_S32K396). Why? and it works?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="seanwu_0-1756431008280.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/354651iAE6F7B271F544ADA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="seanwu_0-1756431008280.png" alt="seanwu_0-1756431008280.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Sean Wu&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 29 Aug 2025 01:33:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-SAR-ADC-resolution/m-p/2160239#M52244</guid>
      <dc:creator>seanwu</dc:creator>
      <dc:date>2025-08-29T01:33:33Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3xx SAR ADC resolution</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-SAR-ADC-resolution/m-p/2160385#M52253</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Sean,&lt;/P&gt;
&lt;P&gt;Section &lt;STRONG&gt;60.2.2 Features&lt;/STRONG&gt; of the &lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K3XXRM" target="_self"&gt;S32K3XXRM&lt;/A&gt; states:&lt;BR /&gt;&lt;FONT color="#808080"&gt;•Selectable resolution (8-, 10-, 12-, &lt;STRONG&gt;14-bit&lt;/STRONG&gt;). Note that the conversion result is always 15 bits wide, even if the selected resolution is smaller (see CALBISTREG[RESN]).&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#808080"&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="60.2.2 Features Selectable resolution (8-, 10-, 12-, 14-bit).png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/354701iD320048C220B6B0C/image-size/large?v=v2&amp;amp;px=999" role="button" title="60.2.2 Features Selectable resolution (8-, 10-, 12-, 14-bit).png" alt="60.2.2 Features Selectable resolution (8-, 10-, 12-, 14-bit).png" /&gt;&lt;/span&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P data-unlink="true"&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/S32K3xx.pdf" target="_self"&gt;S32K3&amp;nbsp;DataSheet&lt;/A&gt;&amp;nbsp;states: TUE spec for precision and standard channels is based on 12-bit level resolution.&lt;BR /&gt;If you set the resolution to 14-bit, the TUE is only slightly better than that of 12-bit resolution.&lt;/P&gt;
&lt;P data-unlink="true"&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 29 Aug 2025 05:59:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-SAR-ADC-resolution/m-p/2160385#M52253</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-08-29T05:59:40Z</dc:date>
    </item>
  </channel>
</rss>