<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: External GPIO interrupt example in S32k3 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/External-GPIO-interrupt-example-in-S32k3/m-p/2160106#M52241</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252204"&gt;@leo_Z&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This HOWTO was implemented using RTD version 2.0.0, and several changes have been introduced in subsequent releases. As a result, some discrepancies may appear when following the instructions with newer versions.&lt;/P&gt;
&lt;P&gt;The Siul2_Icu_Ip_Init() function error message is displayed due to a mismatch in the expected configuration parameter. The parameter passed to the function does not exist under the expected name—it was generated with a different identifier.&lt;/P&gt;
&lt;P&gt;For example, instead of using: &lt;STRONG&gt;Siul2_Icu_Ip_0_Config_PB_BOARD_InitPeripherals&lt;/STRONG&gt;. You should use: &lt;STRONG&gt;Siul2_Icu_Ip_0_Config_PB&lt;/STRONG&gt;. This correct configuration can be found in the Siul2_Icu_Ip_SA_PBcfg.h file.&lt;/P&gt;
&lt;P&gt;For better reference, I recommend reviewing the Siul2_Icu_Ip_BlinkLed_S32K344 example. It implements the same application as described in the HOWTO.&amp;nbsp;This example is included with the RTD package and can be easily accessed when creating a new project from an example&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
    <pubDate>Thu, 28 Aug 2025 17:25:04 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2025-08-28T17:25:04Z</dc:date>
    <item>
      <title>External GPIO interrupt example in S32k3</title>
      <link>https://community.nxp.com/t5/S32K/External-GPIO-interrupt-example-in-S32k3/m-p/2160009#M52237</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I'm trying to execute simple external GPIO interrupt in&amp;nbsp;S32K3X4EVB-Q172 using push button SW5&lt;/P&gt;&lt;P&gt;I'm followed the&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/SIUL2-external-interrupt-example-project-using-S32K3-RTD-without/ta-p/1552335" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/SIUL2-external-interrupt-example-project-using-S32K3-RTD-without/ta-p/1552335&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is main file&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AntoZ_0-1756390127775.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/354602iA71E91A4BDC02CDA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="AntoZ_0-1756390127775.png" alt="AntoZ_0-1756390127775.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;AntoZ_0-1756390127775.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But i'm getting an error as "&lt;SPAN&gt;SIUL2_ICU_IP_INSTANCE" not declared and other errors too&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AntoZ_1-1756390147256.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/354603i4B7EC5002305D261/image-size/medium?v=v2&amp;amp;px=400" role="button" title="AntoZ_1-1756390147256.png" alt="AntoZ_1-1756390147256.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;AntoZ_1-1756390147256.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AntoZ_2-1756390232668.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/354604i84FE10CB5CFC311A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="AntoZ_2-1756390232668.png" alt="AntoZ_2-1756390232668.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;AntoZ_2-1756390232668.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SIUL2 INSTANCE is configured as 0 but its not updated in respected file&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AntoZ_3-1756390319411.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/354605i1C69C4CA823A61D6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="AntoZ_3-1756390319411.png" alt="AntoZ_3-1756390319411.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;AntoZ_3-1756390319411.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Am I missing something in configuration,&lt;/P&gt;&lt;P&gt;Can anyone help this or any example available for GPIO interrupt with push button and led toggle with&amp;nbsp;S32K3X4EVB-Q172 board&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The project folder is attached bellow , I'm using RTD 5.0.0.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 28 Aug 2025 14:15:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/External-GPIO-interrupt-example-in-S32k3/m-p/2160009#M52237</guid>
      <dc:creator>leo_Z</dc:creator>
      <dc:date>2025-08-28T14:15:08Z</dc:date>
    </item>
    <item>
      <title>Re: External GPIO interrupt example in S32k3</title>
      <link>https://community.nxp.com/t5/S32K/External-GPIO-interrupt-example-in-S32k3/m-p/2160106#M52241</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252204"&gt;@leo_Z&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This HOWTO was implemented using RTD version 2.0.0, and several changes have been introduced in subsequent releases. As a result, some discrepancies may appear when following the instructions with newer versions.&lt;/P&gt;
&lt;P&gt;The Siul2_Icu_Ip_Init() function error message is displayed due to a mismatch in the expected configuration parameter. The parameter passed to the function does not exist under the expected name—it was generated with a different identifier.&lt;/P&gt;
&lt;P&gt;For example, instead of using: &lt;STRONG&gt;Siul2_Icu_Ip_0_Config_PB_BOARD_InitPeripherals&lt;/STRONG&gt;. You should use: &lt;STRONG&gt;Siul2_Icu_Ip_0_Config_PB&lt;/STRONG&gt;. This correct configuration can be found in the Siul2_Icu_Ip_SA_PBcfg.h file.&lt;/P&gt;
&lt;P&gt;For better reference, I recommend reviewing the Siul2_Icu_Ip_BlinkLed_S32K344 example. It implements the same application as described in the HOWTO.&amp;nbsp;This example is included with the RTD package and can be easily accessed when creating a new project from an example&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Thu, 28 Aug 2025 17:25:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/External-GPIO-interrupt-example-in-S32k3/m-p/2160106#M52241</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2025-08-28T17:25:04Z</dc:date>
    </item>
  </channel>
</rss>