<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Crypto_43_HSE wrong configuration export</title>
    <link>https://community.nxp.com/t5/S32K/Crypto-43-HSE-wrong-configuration-export/m-p/2159893#M52233</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can tell that the issue seems not to be solved yet.&lt;BR /&gt;Analyzing, for example, the file&amp;nbsp;Crypto_43_HSE_s32k312_hdqfp100.epd that is bundled with the latest Crypto_43_HSE module, you can see that the parameter has upper multiplicity = lower multiplicity = 1:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="strofald_0-1756379227089.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/354575i1A1D7CB7B4D7D69E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="strofald_0-1756379227089.png" alt="strofald_0-1756379227089.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The DaVinci configurator extracts its definition information from this file, and as I said I am forced to have it configured.&lt;/P&gt;</description>
    <pubDate>Thu, 28 Aug 2025 11:08:04 GMT</pubDate>
    <dc:creator>strofald</dc:creator>
    <dc:date>2025-08-28T11:08:04Z</dc:date>
    <item>
      <title>Crypto_43_HSE wrong configuration export</title>
      <link>https://community.nxp.com/t5/S32K/Crypto-43-HSE-wrong-configuration-export/m-p/2089153#M48276</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using Crypto_43_HSE RTD driver v5.0.0.&lt;/P&gt;&lt;P&gt;I configured the driver in EB Tresos and then I executed the exporter to generate the .arxml file to import it into an external tool (DaVinci configurator)&lt;/P&gt;&lt;P&gt;However, it seems that there's something wrong in the way the generator creates the export file. More specifically, the parameter&amp;nbsp;HseKeyCatalogGroupRef is defined&amp;nbsp; in the exported ARXML to have upper multiplicity = lower multiplicity = 1, so it means that this parameter must be always filled in.&lt;/P&gt;&lt;P&gt;However there are cases in which this cannot happen.&lt;/P&gt;&lt;P&gt;For example, when I define the KeyElements SHE Mac Proof and SHE Cipher Proof with KeyElementId=2 and 6 respectively, I do not select the 'Use Hse Key' option because those must not be linked to an HSE key slot , and thus the&amp;nbsp;HseKeyCatalogGroupRef remains empty (and gives me a warning)&amp;nbsp;&lt;BR /&gt;So, since there's this case in which the&amp;nbsp;HseKeyCatalogGroupRef can be empty, I think it's wrong for the exporter to generate the parameter with multiplicity = (1,1) essentially forcing that parameter to always be defined.&lt;BR /&gt;In fact, when I import the configuration through the .arxml file in the DaVinci Configurator, the tool complains about the&amp;nbsp;HseKeyCatalogGroupRef parameter even though it can only be empty for the reasons I explained above.&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;</description>
      <pubDate>Tue, 29 Apr 2025 08:32:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Crypto-43-HSE-wrong-configuration-export/m-p/2089153#M48276</guid>
      <dc:creator>strofald</dc:creator>
      <dc:date>2025-04-29T08:32:48Z</dc:date>
    </item>
    <item>
      <title>Re: Crypto_43_HSE wrong configuration export</title>
      <link>https://community.nxp.com/t5/S32K/Crypto-43-HSE-wrong-configuration-export/m-p/2091358#M48430</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229151"&gt;@strofald&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I'm sorry for delayed response. &lt;/P&gt;
&lt;P&gt;I have asked SW team about this, I will let you know their feedback later. Thanks for patience.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Mon, 05 May 2025 10:27:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Crypto-43-HSE-wrong-configuration-export/m-p/2091358#M48430</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2025-05-05T10:27:10Z</dc:date>
    </item>
    <item>
      <title>Re: Crypto_43_HSE wrong configuration export</title>
      <link>https://community.nxp.com/t5/S32K/Crypto-43-HSE-wrong-configuration-export/m-p/2103149#M49113</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229151"&gt;@strofald&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I'm sorry for delayed response. I just received following feedback:&lt;/P&gt;
&lt;P&gt;"&lt;SPAN&gt;The development team has confirmed that in the&amp;nbsp;latest codebase, the multiplicity for&amp;nbsp;HseKeyCatalogGroupRef&amp;nbsp;is correctly configured to allow it to be&amp;nbsp;optional.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN data-immersive-translate-walked="1abf4617-bac2-4fdd-ad94-83c072bfef0a"&gt;This means&amp;nbsp; multiplicity valid, and allowing the field to be left empty when not applicable.&amp;nbsp;&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;"&lt;STRONG data-immersive-translate-walked="1abf4617-bac2-4fdd-ad94-83c072bfef0a" data-immersive-translate-paragraph="1"&gt;In crypto configuration there is no multiplicity added to HseKeyCatalogGroupRef, and tool itself is adding lower and upper multiplicity to one by default.&lt;/STRONG&gt;"&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 23 May 2025 05:25:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Crypto-43-HSE-wrong-configuration-export/m-p/2103149#M49113</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2025-05-23T05:25:01Z</dc:date>
    </item>
    <item>
      <title>Re: Crypto_43_HSE wrong configuration export</title>
      <link>https://community.nxp.com/t5/S32K/Crypto-43-HSE-wrong-configuration-export/m-p/2159893#M52233</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can tell that the issue seems not to be solved yet.&lt;BR /&gt;Analyzing, for example, the file&amp;nbsp;Crypto_43_HSE_s32k312_hdqfp100.epd that is bundled with the latest Crypto_43_HSE module, you can see that the parameter has upper multiplicity = lower multiplicity = 1:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="strofald_0-1756379227089.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/354575i1A1D7CB7B4D7D69E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="strofald_0-1756379227089.png" alt="strofald_0-1756379227089.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The DaVinci configurator extracts its definition information from this file, and as I said I am forced to have it configured.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Aug 2025 11:08:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Crypto-43-HSE-wrong-configuration-export/m-p/2159893#M52233</guid>
      <dc:creator>strofald</dc:creator>
      <dc:date>2025-08-28T11:08:04Z</dc:date>
    </item>
  </channel>
</rss>