<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K142 Csec FlashPartition run in ram</title>
    <link>https://community.nxp.com/t5/S32K/S32K142-Csec-FlashPartition-run-in-ram/m-p/2158057#M52150</link>
    <description>&lt;P&gt;Yes, it is needed to do it in steps with reset in between.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 26 Aug 2025 06:29:27 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2025-08-26T06:29:27Z</dc:date>
    <item>
      <title>S32K142 Csec FlashPartition run in ram</title>
      <link>https://community.nxp.com/t5/S32K/S32K142-Csec-FlashPartition-run-in-ram/m-p/2156552#M52077</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Now i used SDK RTM v4.0.2 Example Project about "csec_keyconfig“，In initFlashForCsecOperation&amp;nbsp;Function montioned&amp;nbsp;Flash partitioning for CSEc operation must only be ran with RAM configuration.&lt;/P&gt;&lt;P&gt;1.can i run some function in ram such as&amp;nbsp;FLASH_DRV_DEFlashPartition，FLASH_DRV_CommandSequence ... or all project run in ram？&lt;/P&gt;</description>
      <pubDate>Fri, 22 Aug 2025 06:57:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K142-Csec-FlashPartition-run-in-ram/m-p/2156552#M52077</guid>
      <dc:creator>top</dc:creator>
      <dc:date>2025-08-22T06:57:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32K142 Csec FlashPartition run in ram</title>
      <link>https://community.nxp.com/t5/S32K/S32K142-Csec-FlashPartition-run-in-ram/m-p/2156777#M52092</link>
      <description>&lt;P&gt;This needs only first time to run from RAM (as flash partitioning needs to be done only once), so may run the whole project from RAM.&lt;/P&gt;
&lt;P&gt;But in principle only flashing routines needs to run from RAM to avoid read-while-write issues.&lt;/P&gt;</description>
      <pubDate>Fri, 22 Aug 2025 13:01:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K142-Csec-FlashPartition-run-in-ram/m-p/2156777#M52092</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2025-08-22T13:01:06Z</dc:date>
    </item>
    <item>
      <title>Re: S32K142 Csec FlashPartition run in ram</title>
      <link>https://community.nxp.com/t5/S32K/S32K142-Csec-FlashPartition-run-in-ram/m-p/2157437#M52125</link>
      <description>&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;but&amp;nbsp;When conducting quantity production, is it necessary to first burn a program that runs entirely in RAM to partition Flash, and then burn the app？&lt;/P&gt;</description>
      <pubDate>Mon, 25 Aug 2025 08:37:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K142-Csec-FlashPartition-run-in-ram/m-p/2157437#M52125</guid>
      <dc:creator>top</dc:creator>
      <dc:date>2025-08-25T08:37:26Z</dc:date>
    </item>
    <item>
      <title>Re: S32K142 Csec FlashPartition run in ram</title>
      <link>https://community.nxp.com/t5/S32K/S32K142-Csec-FlashPartition-run-in-ram/m-p/2158057#M52150</link>
      <description>&lt;P&gt;Yes, it is needed to do it in steps with reset in between.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Aug 2025 06:29:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K142-Csec-FlashPartition-run-in-ram/m-p/2158057#M52150</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2025-08-26T06:29:27Z</dc:date>
    </item>
  </channel>
</rss>