<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic EEPROM write and read in s32k while device is secure in S32K</title>
    <link>https://community.nxp.com/t5/S32K/EEPROM-write-and-read-in-s32k-while-device-is-secure/m-p/2156022#M52047</link>
    <description>&lt;P&gt;I tried writing and reading to the EEPROM, and it works when the device is unsecure. However, after enabling device security through the FSEC bit and flashing the hex file, the EEPROM stops working.&lt;/P&gt;</description>
    <pubDate>Thu, 21 Aug 2025 11:02:01 GMT</pubDate>
    <dc:creator>Saranraj</dc:creator>
    <dc:date>2025-08-21T11:02:01Z</dc:date>
    <item>
      <title>EEPROM write and read in s32k while device is secure</title>
      <link>https://community.nxp.com/t5/S32K/EEPROM-write-and-read-in-s32k-while-device-is-secure/m-p/2156022#M52047</link>
      <description>&lt;P&gt;I tried writing and reading to the EEPROM, and it works when the device is unsecure. However, after enabling device security through the FSEC bit and flashing the hex file, the EEPROM stops working.&lt;/P&gt;</description>
      <pubDate>Thu, 21 Aug 2025 11:02:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/EEPROM-write-and-read-in-s32k-while-device-is-secure/m-p/2156022#M52047</guid>
      <dc:creator>Saranraj</dc:creator>
      <dc:date>2025-08-21T11:02:01Z</dc:date>
    </item>
    <item>
      <title>Re: EEPROM write and read in s32k while device is secure</title>
      <link>https://community.nxp.com/t5/S32K/EEPROM-write-and-read-in-s32k-while-device-is-secure/m-p/2156573#M52078</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217037"&gt;@Saranraj&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The Flash Configuration Field can also set protection for the Emulated EEPROM.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1755846780840.png" style="width: 551px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/353647iC76B2BBF52478A73/image-dimensions/551x292?v=v2" width="551" height="292" role="button" title="danielmartynek_0-1755846780840.png" alt="danielmartynek_0-1755846780840.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Do you have a communication interface that can be used to send the content of the 0x400-0x40F memory out while the MCU is secure?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Aug 2025 07:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/EEPROM-write-and-read-in-s32k-while-device-is-secure/m-p/2156573#M52078</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-08-22T07:15:58Z</dc:date>
    </item>
  </channel>
</rss>