<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CAN Example on S32K14W-Q064 rerefence board in S32K</title>
    <link>https://community.nxp.com/t5/S32K/CAN-Example-on-S32K14W-Q064-rerefence-board/m-p/2154286#M51946</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188029"&gt;@Senlent&lt;/a&gt;&amp;nbsp;thanks for your reply. I have one more question.&lt;BR /&gt;&lt;BR /&gt;I found&amp;nbsp;UJA1169TK(CAN0) and TJA1145(CAN1) as CAN tranceiver on the reference board(&lt;SPAN&gt;S32K14W-Q064).&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Do these devices require any additional configuration for CAN communication? If so, could you share any relevant modules or example code?&lt;BR /&gt;&lt;BR /&gt;Thanks in advnace.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 19 Aug 2025 09:19:36 GMT</pubDate>
    <dc:creator>vincent841</dc:creator>
    <dc:date>2025-08-19T09:19:36Z</dc:date>
    <item>
      <title>CAN Example on S32K14W-Q064 rerefence board</title>
      <link>https://community.nxp.com/t5/S32K/CAN-Example-on-S32K14W-Q064-rerefence-board/m-p/2154075#M51937</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I'm testing CAN communication on S32K14W-Q064 reference board. I'm using S32DS version 3.6.3 and AUTOSAR R21-11 RTD 3.0.0 recommended by here.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to check some examples like 'CAN_example_S32K144W' and 'FlexCAN_Ip_example_S32K144W' but it doesn't work.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you give me some information like additional configurations or test codes?&amp;nbsp; Thanks in advance.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Aug 2025 06:06:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-Example-on-S32K14W-Q064-rerefence-board/m-p/2154075#M51937</guid>
      <dc:creator>vincent841</dc:creator>
      <dc:date>2025-08-19T06:06:16Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Example on S32K14W-Q064 rerefence board</title>
      <link>https://community.nxp.com/t5/S32K/CAN-Example-on-S32K14W-Q064-rerefence-board/m-p/2154250#M51943</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@vincent841" target="_blank"&gt;Hi@vincent841&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;the demo "&lt;SPAN&gt;FlexCAN_Ip_example_S32K144W&lt;/SPAN&gt;" work in flexcan loop-back mode, you need to do some modification&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1.change flexcan0 work mode to normal,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2.add port for flexcan0&lt;/P&gt;</description>
      <pubDate>Tue, 19 Aug 2025 08:54:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-Example-on-S32K14W-Q064-rerefence-board/m-p/2154250#M51943</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2025-08-19T08:54:46Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Example on S32K14W-Q064 rerefence board</title>
      <link>https://community.nxp.com/t5/S32K/CAN-Example-on-S32K14W-Q064-rerefence-board/m-p/2154286#M51946</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188029"&gt;@Senlent&lt;/a&gt;&amp;nbsp;thanks for your reply. I have one more question.&lt;BR /&gt;&lt;BR /&gt;I found&amp;nbsp;UJA1169TK(CAN0) and TJA1145(CAN1) as CAN tranceiver on the reference board(&lt;SPAN&gt;S32K14W-Q064).&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Do these devices require any additional configuration for CAN communication? If so, could you share any relevant modules or example code?&lt;BR /&gt;&lt;BR /&gt;Thanks in advnace.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Aug 2025 09:19:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-Example-on-S32K14W-Q064-rerefence-board/m-p/2154286#M51946</guid>
      <dc:creator>vincent841</dc:creator>
      <dc:date>2025-08-19T09:19:36Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Example on S32K14W-Q064 rerefence board</title>
      <link>https://community.nxp.com/t5/S32K/CAN-Example-on-S32K14W-Q064-rerefence-board/m-p/2154312#M51949</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@vincent841" target="_blank"&gt;Hi@vincent841&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The UJA116x's CAN features are enabled by default, so you don't need to configure them to evaluate CAN feature.&lt;/P&gt;
&lt;P&gt;The TJA1145 requires configuration, but I don't have driver example code for this transceiver.&lt;/P&gt;
&lt;P&gt;If you have questions related to the UJA116x or JTA1145, please create a new topic.&lt;/P&gt;</description>
      <pubDate>Tue, 19 Aug 2025 09:46:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-Example-on-S32K14W-Q064-rerefence-board/m-p/2154312#M51949</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2025-08-19T09:46:46Z</dc:date>
    </item>
  </channel>
</rss>