<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: C40 Code Memory Allocation – Hard Fault When Changing Sector in S32K</title>
    <link>https://community.nxp.com/t5/S32K/C40-Code-Memory-Allocation-Hard-Fault-When-Changing-Sector/m-p/2151396#M51809</link>
    <description>&lt;P&gt;Hi@&lt;SPAN&gt;GaneshBhagwat&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;This should be an Read-While-Write Event Error(RWE), you need to put flash operation into SRAM to avoid RWE.&lt;/P&gt;
&lt;P&gt;Please refer to this post:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K312-C40-Ip-SRAM-RTD-500-DS35/ta-p/2074245" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K312-C40-Ip-SRAM-RTD-500-DS35/ta-p/2074245&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 13 Aug 2025 06:29:53 GMT</pubDate>
    <dc:creator>Senlent</dc:creator>
    <dc:date>2025-08-13T06:29:53Z</dc:date>
    <item>
      <title>C40 Code Memory Allocation – Hard Fault When Changing Sector</title>
      <link>https://community.nxp.com/t5/S32K/C40-Code-Memory-Allocation-Hard-Fault-When-Changing-Sector/m-p/2151017#M51794</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I’m working with the C40 flash memory driver and used the following configuration, which works fine with the default project settings:&lt;/P&gt;&lt;PRE&gt;#define EXAMPLE_MASTER_ID         (0U)
#define EXAMPLE_SECTOR_START_ADDR (0x00600000U)
#define EXAMPLE_SECTOR_TEST       (C40_CODE_ARRAY_0_BLOCK_1_S256)
#define EXAMPLE_BUFFER_SIZE       (64U) // or 128U&lt;/PRE&gt;&lt;P&gt;However, when I change the settings to:&lt;/P&gt;&lt;PRE&gt;#define EXAMPLE_MASTER_ID         (0U)
#define EXAMPLE_SECTOR_START_ADDR (0x00500000U)
#define EXAMPLE_SECTOR_TEST       (C40_CODE_ARRAY_0_BLOCK_0_S128)
#define EXAMPLE_BUFFER_SIZE       (64U) // or 128U&lt;/PRE&gt;&lt;P&gt;the program hits a &lt;STRONG&gt;hard fault&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Could anyone clarify what might cause this issue?&lt;BR /&gt;From my understanding, possible causes could be:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;The selected start address overlaps with a protected or reserved flash region.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;The sector/block size definition (C40_CODE_ARRAY_0_BLOCK_0_S128) doesn’t match the actual memory map for the device.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Attempting to write or erase from a block where the code is currently executing.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Misalignment with the flash controller’s sector boundaries.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I’ve attached an image showing the issue in more detail.&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Ganesh Bhagwat&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Aug 2025 16:26:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/C40-Code-Memory-Allocation-Hard-Fault-When-Changing-Sector/m-p/2151017#M51794</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2025-08-12T16:26:39Z</dc:date>
    </item>
    <item>
      <title>Re: C40 Code Memory Allocation – Hard Fault When Changing Sector</title>
      <link>https://community.nxp.com/t5/S32K/C40-Code-Memory-Allocation-Hard-Fault-When-Changing-Sector/m-p/2151396#M51809</link>
      <description>&lt;P&gt;Hi@&lt;SPAN&gt;GaneshBhagwat&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;This should be an Read-While-Write Event Error(RWE), you need to put flash operation into SRAM to avoid RWE.&lt;/P&gt;
&lt;P&gt;Please refer to this post:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K312-C40-Ip-SRAM-RTD-500-DS35/ta-p/2074245" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K312-C40-Ip-SRAM-RTD-500-DS35/ta-p/2074245&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Aug 2025 06:29:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/C40-Code-Memory-Allocation-Hard-Fault-When-Changing-Sector/m-p/2151396#M51809</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2025-08-13T06:29:53Z</dc:date>
    </item>
  </channel>
</rss>