<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ADC initialization for S32K311 microcontroller in S32K</title>
    <link>https://community.nxp.com/t5/S32K/ADC-initialization-for-S32K311-microcontroller/m-p/2150873#M51789</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is there any delay time required for ADC initialization?&lt;/P&gt;&lt;P&gt;Because, on first ADC conversion, I am observing incorrect ADC values when I am giving a delay of less than 10ms where as when I am giving a delay of 10ms then the ADC values are correct.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am facing this issue for Pin PTA10 and PTC5 for above mentioned microcontroller where these were JTAG pin which are configured as GPIO pins&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 12 Aug 2025 11:06:03 GMT</pubDate>
    <dc:creator>truptikavadi1</dc:creator>
    <dc:date>2025-08-12T11:06:03Z</dc:date>
    <item>
      <title>ADC initialization for S32K311 microcontroller</title>
      <link>https://community.nxp.com/t5/S32K/ADC-initialization-for-S32K311-microcontroller/m-p/2150873#M51789</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is there any delay time required for ADC initialization?&lt;/P&gt;&lt;P&gt;Because, on first ADC conversion, I am observing incorrect ADC values when I am giving a delay of less than 10ms where as when I am giving a delay of 10ms then the ADC values are correct.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am facing this issue for Pin PTA10 and PTC5 for above mentioned microcontroller where these were JTAG pin which are configured as GPIO pins&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Aug 2025 11:06:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC-initialization-for-S32K311-microcontroller/m-p/2150873#M51789</guid>
      <dc:creator>truptikavadi1</dc:creator>
      <dc:date>2025-08-12T11:06:03Z</dc:date>
    </item>
    <item>
      <title>Re: ADC initialization for S32K311 microcontroller</title>
      <link>https://community.nxp.com/t5/S32K/ADC-initialization-for-S32K311-microcontroller/m-p/2156360#M52066</link>
      <description>&lt;P&gt;Thank you for your interest in our products and for contributing to our community.&lt;/P&gt;
&lt;P&gt;I must admit that I have not tried analog readings on JTAG pins, since we do not have them available in the headers of our EVBs.&lt;/P&gt;
&lt;P&gt;Also consider that at least these pins are connected to pull-up resistors for JTAG configuration.&lt;/P&gt;
&lt;P&gt;In addition to the RTD examples, I recommend checking out the following examples:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32M-Knowledge-Base/S32M27x-S32K3-eMIOS-BTCU-ADC-DMA-RTD600/ta-p/2155542" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/S32M-Knowledge-Base/S32M27x-S32K3-eMIOS-BTCU-ADC-DMA-RTD600/ta-p/2155542&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/RTD400-LLD-K344-ADC-SW-HW-trigger/ta-p/1966179" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/RTD400-LLD-K344-ADC-SW-HW-trigger/ta-p/1966179&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I hope this information is helpful.&lt;/P&gt;</description>
      <pubDate>Thu, 21 Aug 2025 23:27:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC-initialization-for-S32K311-microcontroller/m-p/2156360#M52066</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2025-08-21T23:27:41Z</dc:date>
    </item>
  </channel>
</rss>