<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic flexcan MAXMB in S32K</title>
    <link>https://community.nxp.com/t5/S32K/flexcan-MAXMB/m-p/2149743#M51721</link>
    <description>&lt;P&gt;hello:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;have a question about numbers of the mailbox.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;for 32k1XX's flexcan, the total number of MBs will be different when&amp;nbsp;payload sizes are different. it's described that MAXMB bits in Module Configuration register (MCR)must&amp;nbsp;programmed with a value smaller than or equal to the number of available message buffers.&amp;nbsp; if MAXMB is programmed with a value bigger than&amp;nbsp;the number of available message buffers, what will happen? for example, use a 32-byte playload but set the MAXMB to 32.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR!&lt;/P&gt;</description>
    <pubDate>Mon, 11 Aug 2025 05:38:30 GMT</pubDate>
    <dc:creator>fan1234</dc:creator>
    <dc:date>2025-08-11T05:38:30Z</dc:date>
    <item>
      <title>flexcan MAXMB</title>
      <link>https://community.nxp.com/t5/S32K/flexcan-MAXMB/m-p/2149743#M51721</link>
      <description>&lt;P&gt;hello:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;have a question about numbers of the mailbox.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;for 32k1XX's flexcan, the total number of MBs will be different when&amp;nbsp;payload sizes are different. it's described that MAXMB bits in Module Configuration register (MCR)must&amp;nbsp;programmed with a value smaller than or equal to the number of available message buffers.&amp;nbsp; if MAXMB is programmed with a value bigger than&amp;nbsp;the number of available message buffers, what will happen? for example, use a 32-byte playload but set the MAXMB to 32.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR!&lt;/P&gt;</description>
      <pubDate>Mon, 11 Aug 2025 05:38:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/flexcan-MAXMB/m-p/2149743#M51721</guid>
      <dc:creator>fan1234</dc:creator>
      <dc:date>2025-08-11T05:38:30Z</dc:date>
    </item>
    <item>
      <title>Re: flexcan MAXMB</title>
      <link>https://community.nxp.com/t5/S32K/flexcan-MAXMB/m-p/2149862#M51728</link>
      <description>&lt;P&gt;Hi@&lt;SPAN&gt;fan1234&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;There is no need to discuss this. The FlexCAN module does not have such a large SRAM space. Your access is out of bounds and you are accessing a non-existent address space.&lt;/P&gt;</description>
      <pubDate>Mon, 11 Aug 2025 08:05:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/flexcan-MAXMB/m-p/2149862#M51728</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2025-08-11T08:05:00Z</dc:date>
    </item>
  </channel>
</rss>