<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: CAN FD and CAN(not Working)</title>
    <link>https://community.nxp.com/t5/S32K/CAN-FD-and-CAN-not-Working/m-p/2146989#M51615</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi Julián,&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;I initially suspected a software configuration issue, which is why I posted here. However, it turned out to be a hardware-related problem with the TJA1443 transceiver connection. Due to a floating pin, I was unable to receive or transmit any CAN messages in normal CAN but I don't know why it was working in FD.&lt;/P&gt;&lt;P&gt;After resolving the hardware issue, everything is now working as expected.&lt;/P&gt;&lt;P&gt;Thanks again for taking the time to respond and for pointing me toward the helpful community post.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Ganesh&lt;/P&gt;</description>
    <pubDate>Tue, 05 Aug 2025 16:36:05 GMT</pubDate>
    <dc:creator>GaneshBhagwat</dc:creator>
    <dc:date>2025-08-05T16:36:05Z</dc:date>
    <item>
      <title>CAN FD and CAN(not Working)</title>
      <link>https://community.nxp.com/t5/S32K/CAN-FD-and-CAN-not-Working/m-p/2141012#M51342</link>
      <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;I'm currently facing an issue with my CAN configuration. I'm using a basic setup for CAN communication, and it only works when I use &lt;STRONG&gt;CAN-FD mode&lt;/STRONG&gt; with &lt;STRONG&gt;PEAK CAN Viewer&lt;/STRONG&gt;. However, when I try standard &lt;STRONG&gt;Classical CAN&lt;/STRONG&gt; (non-FD), I do not receive any response.&lt;/P&gt;&lt;P&gt;I've attached my project for reference. Could someone kindly review it and let me know if there might be any missing configuration or setting that I’ve overlooked?&lt;/P&gt;&lt;P&gt;To summarize:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;CAN-FD + PEAK CAN Viewer&lt;/STRONG&gt;: Working as expected&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Standard CAN + PEAK CAN Viewer&lt;/STRONG&gt;: No response from the board&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Any suggestions or guidance would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Ganesh Bhagwat&lt;/P&gt;</description>
      <pubDate>Fri, 25 Jul 2025 15:33:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-FD-and-CAN-not-Working/m-p/2141012#M51342</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2025-07-25T15:33:41Z</dc:date>
    </item>
    <item>
      <title>Re: CAN FD and CAN(not Working)</title>
      <link>https://community.nxp.com/t5/S32K/CAN-FD-and-CAN-not-Working/m-p/2142901#M51439</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244803"&gt;@GaneshBhagwat&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Is the PCAN-View tool configured correctly for the mode, baud rate and sampling point?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Is it possible to share what do you see on the bus? (By using a logic analyzer or oscilloscope) just to confirm if the frame is being sent correctly. Also, please elaborate on what "not working" implies; are you able to enter callback upon reception? Is it only transmissions you are having issues with?&lt;/P&gt;
&lt;P&gt;I can see in your CANInit function, ID 0x80000 is being set for acceptance, confirm if this is also set in the CAN analyzer.&lt;/P&gt;
&lt;P&gt;You can use this community post as guidance for CAN configuration:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K358-FlexCAN-TXRX-ISR-S32DS35-RTD400-500/ta-p/1981987" target="_blank"&gt;Example S32K358 FlexCAN TXRX ISR S32DS35 RTD400/500 - NXP Community&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Tue, 29 Jul 2025 18:32:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-FD-and-CAN-not-Working/m-p/2142901#M51439</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-07-29T18:32:01Z</dc:date>
    </item>
    <item>
      <title>Re: CAN FD and CAN(not Working)</title>
      <link>https://community.nxp.com/t5/S32K/CAN-FD-and-CAN-not-Working/m-p/2146989#M51615</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi Julián,&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;I initially suspected a software configuration issue, which is why I posted here. However, it turned out to be a hardware-related problem with the TJA1443 transceiver connection. Due to a floating pin, I was unable to receive or transmit any CAN messages in normal CAN but I don't know why it was working in FD.&lt;/P&gt;&lt;P&gt;After resolving the hardware issue, everything is now working as expected.&lt;/P&gt;&lt;P&gt;Thanks again for taking the time to respond and for pointing me toward the helpful community post.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Ganesh&lt;/P&gt;</description>
      <pubDate>Tue, 05 Aug 2025 16:36:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-FD-and-CAN-not-Working/m-p/2146989#M51615</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2025-08-05T16:36:05Z</dc:date>
    </item>
  </channel>
</rss>