<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32K324 ADC resolution bit</title>
    <link>https://community.nxp.com/t5/S32K/S32K324-ADC-resolution-bit/m-p/2144429#M51515</link>
    <description>&lt;P&gt;Selectable resolution (8-, 10-, 12-, 14-bit).&lt;BR /&gt;However, please note that the TUE spec for precision and standard channels is based on 12-bit level resolution.&lt;/P&gt;</description>
    <pubDate>Thu, 31 Jul 2025 09:25:08 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2025-07-31T09:25:08Z</dc:date>
    <item>
      <title>S32K324 ADC resolution bit</title>
      <link>https://community.nxp.com/t5/S32K/S32K324-ADC-resolution-bit/m-p/1837571#M33609</link>
      <description>&lt;P&gt;Hello, I would like to ask a question. I am using a chip, S32K324, and the AD written on the chip is 12 bits. However, in the manual, the CALLISTREG register can select 4 different bits, 14 bit, 12 bit, 10 bit, and 8 bit. How do I understand this? Isn't the conversion result always 12 bits? How many bits for S channel, P channel, and X channel, respectively? Thank you!&lt;/P&gt;</description>
      <pubDate>Fri, 29 Mar 2024 02:41:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K324-ADC-resolution-bit/m-p/1837571#M33609</guid>
      <dc:creator>jack_22</dc:creator>
      <dc:date>2024-03-29T02:41:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32K324 ADC resolution bit</title>
      <link>https://community.nxp.com/t5/S32K/S32K324-ADC-resolution-bit/m-p/1838794#M33690</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;The 12-bit resolution is officially supported, there are specs in the Data Sheet based on that.&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;Conversion data is always 15bits wide, regardless of the conversion resolution selected (14, 12, 10, 8 significant bits per conversion data, reducing this number speeds up the conversion because the SAR algorithm executes fewer steps).&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="2.1. ADC basic concepts AN13413.png" style="width: 820px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/271387i85DADA122740B2E2/image-size/large?v=v2&amp;amp;px=999" role="button" title="2.1. ADC basic concepts AN13413.png" alt="2.1. ADC basic concepts AN13413.png" /&gt;&lt;/span&gt;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;How many bits for S channel, P channel, and X channel, respectively? &lt;/EM&gt;The resolutions of the three types of ADC channels are the same.&amp;nbsp;Due to the difference between Pin capacitance, Analog Bus Capacitance, and Channel selection Switch impedance, Precision channel&amp;nbsp;is more accurate.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 01 Apr 2024 23:47:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K324-ADC-resolution-bit/m-p/1838794#M33690</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-04-01T23:47:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32K324 ADC resolution bit</title>
      <link>https://community.nxp.com/t5/S32K/S32K324-ADC-resolution-bit/m-p/2144391#M51513</link>
      <description>&lt;P&gt;&lt;SPAN&gt;"The 12-bit resolution is officially supported"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What do you mean&amp;nbsp;&lt;SPAN&gt;officially&amp;nbsp;supported? It is really confusing that datasheet says 12-bit. Is there any kind of scaling on HW layer?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 31 Jul 2025 08:58:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K324-ADC-resolution-bit/m-p/2144391#M51513</guid>
      <dc:creator>ustaufuk</dc:creator>
      <dc:date>2025-07-31T08:58:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32K324 ADC resolution bit</title>
      <link>https://community.nxp.com/t5/S32K/S32K324-ADC-resolution-bit/m-p/2144429#M51515</link>
      <description>&lt;P&gt;Selectable resolution (8-, 10-, 12-, 14-bit).&lt;BR /&gt;However, please note that the TUE spec for precision and standard channels is based on 12-bit level resolution.&lt;/P&gt;</description>
      <pubDate>Thu, 31 Jul 2025 09:25:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K324-ADC-resolution-bit/m-p/2144429#M51515</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-07-31T09:25:08Z</dc:date>
    </item>
  </channel>
</rss>