<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K344 CAN receive</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-CAN-receive/m-p/2141118#M51347</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/173294"&gt;@toru88&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You are right. I tested your project and the correct definitions for the main function RW periods are not being generated. However, this issue seems to be fixed in version 6.0.0 (RTD package I am currently using). Are you able to update the RTD to the newer versions?&lt;/P&gt;
&lt;P&gt;If not, you can simply edit the &lt;STRONG&gt;Can_43_FLEXCAN_Cfg.h&lt;/STRONG&gt; file like below.&lt;/P&gt;
&lt;P&gt;From this:&lt;/P&gt;
&lt;LI-CODE lang="c"&gt;/**
*   @brief      Period for cyclic call of Main Function Read/Write
*/
#define CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_0    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_1    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_2    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_3    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_4    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_5    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_MULTIPLE_WRITE    (STD_ON)
#define CAN_43_FLEXCAN_MAINFUNCTION_MULTIPLE_READ    (STD_ON)&lt;/LI-CODE&gt;
&lt;P&gt;To this:&lt;/P&gt;
&lt;LI-CODE lang="c"&gt;/**
*   @brief      Period for cyclic call of Main Function Read/Write
*/
#define CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_CanMainFunctionRWPeriods_0    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_CanMainFunctionRWPeriods_1    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_CanMainFunctionRWPeriods_2    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_CanMainFunctionRWPeriods_3    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_CanMainFunctionRWPeriods_4    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_CanMainFunctionRWPeriods_5    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_MULTIPLE_WRITE    (STD_ON)
#define CAN_43_FLEXCAN_MAINFUNCTION_MULTIPLE_READ    (STD_ON)&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 25 Jul 2025 22:32:32 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2025-07-25T22:32:32Z</dc:date>
    <item>
      <title>S32K344 CAN receive</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-receive/m-p/2135960#M51024</link>
      <description>&lt;P&gt;Referring to the “Can_Example_S32K344” sample project.&lt;/P&gt;&lt;P&gt;CAN_43_FLEXCAN_MAINFUNCTION_MULTIPLE_WRITE“ becomes ‘STD_ON’ and ”Can_43_FLEXCAN_MainFunction_Read" is disabled, so CAN reception is not possible.&lt;BR /&gt;Can_43_FLEXCAN_MainFunction_Read_CanMainFunctionRWPeriods_0" is not enabled.&lt;BR /&gt;I have set up 3 channels, “FLEXCAN_0”, ‘FLEXCAN_2’ and “FLEXCAN_5”.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="CAN_43_FLEXCAN_setting_07.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/348093i0BB981BBDAFC31D5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="CAN_43_FLEXCAN_setting_07.png" alt="CAN_43_FLEXCAN_setting_07.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;CAN_43_FLEXCAN_setting_07.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="CAN_43_FLEXCAN_setting_06.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/348094iE950360BC0AB1DF1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="CAN_43_FLEXCAN_setting_06.png" alt="CAN_43_FLEXCAN_setting_06.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;CAN_43_FLEXCAN_setting_06.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="CAN_43_FLEXCAN_setting_05.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/348096iA5E01E903D1896C1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="CAN_43_FLEXCAN_setting_05.png" alt="CAN_43_FLEXCAN_setting_05.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;CAN_43_FLEXCAN_setting_05.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="CAN_43_FLEXCAN_setting_03.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/348099i725644E40868A1F6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="CAN_43_FLEXCAN_setting_03.png" alt="CAN_43_FLEXCAN_setting_03.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;CAN_43_FLEXCAN_setting_03.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="CAN_43_FLEXCAN_setting_02.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/348095iB077D6CF2E5FBE12/image-size/medium?v=v2&amp;amp;px=400" role="button" title="CAN_43_FLEXCAN_setting_02.png" alt="CAN_43_FLEXCAN_setting_02.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;CAN_43_FLEXCAN_setting_02.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="CAN_43_FLEXCAN_setting_01.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/348098i92E0B24FCA229EE7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="CAN_43_FLEXCAN_setting_01.png" alt="CAN_43_FLEXCAN_setting_01.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;CAN_43_FLEXCAN_setting_01.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="CAN_43_FLEXCAN_setting_04.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/348097i9EC3358B33A68373/image-size/medium?v=v2&amp;amp;px=400" role="button" title="CAN_43_FLEXCAN_setting_04.png" alt="CAN_43_FLEXCAN_setting_04.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;CAN_43_FLEXCAN_setting_04.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;       &lt;/P&gt;&lt;P&gt;Attached is the “Can_43_FLEXCAN” setting screen for “FLEXCAN_0”.&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jul 2025 16:11:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-receive/m-p/2135960#M51024</guid>
      <dc:creator>toru88</dc:creator>
      <dc:date>2025-07-17T16:11:22Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 CAN receive</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-receive/m-p/2136065#M51030</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/173294"&gt;@toru88&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you share additional information? Are you having issues with FlexCAN reception? You mentioned "&lt;SPAN&gt;”Can_43_FLEXCAN_MainFunction_Read" is disabled, so CAN reception is not possible.", are you unable to read frames in your main code?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If possible, please share your project (or the main.c file) so I can understand what your routine is.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Additionally, y&lt;/SPAN&gt;ou can refer to the examples in the RTD. They are the same as shown in this training presentation:&amp;nbsp;&lt;A href="https://www.google.com/url?sa=t&amp;amp;rct=j&amp;amp;q=&amp;amp;esrc=s&amp;amp;source=web&amp;amp;cd=&amp;amp;ved=2ahUKEwixvers5cSOAxUPLtAFHak4DXoQFnoECBgQAQ&amp;amp;url=https%3A%2F%2Fcommunity.nxp.com%2Fpwmxy87654%2Fattachments%2Fpwmxy87654%2FS32K%2F44963%2F2%2FS32K3_RTD_Training_CAN%2520(2).pdf&amp;amp;usg=AOvVaw0WaRiQYlS2l7p6VQ5iRDID&amp;amp;opi=89978449" target="_self" rel="nofollow noopener noreferrer"&gt;S32K3XX COMMUNICATION MODULES: FLEXCAN WITH RTD AND LOW-LEVEL DRIVERS.&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;These projects are configured for loopback, so you will need to enable normal/user mode and initialize the transceiver output pins (CAN_H &amp;amp; CAN_L).&lt;/P&gt;
&lt;P&gt;There are also some community posts with examples:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-DMA-test-S32DS3-5/ta-p/2015832" target="_blank" rel="noopener"&gt;Example S32K344 FlexCAN_Ip TX/RX/EnhanceRXFIFO DMA test S32DS3.5 RTD400 - NXP Community&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K344-EVB-With-MCAL-FLEXCAN-TJA1153/td-p/1540687" target="_blank" rel="noopener"&gt;Solved: S32K344 EVB With MCAL FLEXCAN TJA1153 - NXP Community&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jul 2025 22:37:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-receive/m-p/2136065#M51030</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-07-17T22:37:15Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 CAN receive</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-receive/m-p/2136105#M51031</link>
      <description>&lt;P&gt;Hi Julián_AragónM&lt;BR /&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;'CAN_43_FLEXCAN_MAINFUNCTION_MULTIPLE_WRITE' becomes ‘STD_ON’ and ”Can_43_FLEXCAN_MainFunction_Read' is removed from the compilation target.&lt;BR /&gt;Below defines are not done.&lt;BR /&gt;- CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_CanMainFunctionRWPeriods_0&lt;BR /&gt;- CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_CanMainFunctionRWPeriods_1&lt;BR /&gt;- CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_CanMainFunctionRWPeriods_2&lt;/P&gt;&lt;P&gt;The following function is not enabled because this define is not set.&lt;BR /&gt;Therefore, a build error occurs in the code called in Main.&lt;BR /&gt;- Can_43_FLEXCAN_MainFunction_Read_CanMainFunctionRWPeriods_0&lt;BR /&gt;- Can_43_FLEXCAN_MainFunction_Read_CanMainFunctionRWPeriods_1&lt;BR /&gt;- Can_43_FLEXCAN_MainFunction_Read_CanMainFunctionRWPeriods_2&lt;/P&gt;&lt;P&gt;The code is not yet working and cannot be built.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;toru88&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Jul 2025 00:33:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-receive/m-p/2136105#M51031</guid>
      <dc:creator>toru88</dc:creator>
      <dc:date>2025-07-18T00:33:17Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 CAN receive</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-receive/m-p/2137654#M51158</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/173294"&gt;@toru88&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;When only 1 RW period is defined, a single function is used for polling:&lt;/P&gt;
&lt;LI-CODE lang="c"&gt;void Can_43_FLEXCAN_MainFunction_Read(void);&lt;/LI-CODE&gt;
&lt;P&gt;On the other hand, when multiple periods are defined, multiple polling functions are defined for different timing requirements:&lt;/P&gt;
&lt;LI-CODE lang="c"&gt;void Can_43_FLEXCAN_MainFunction_Read_CanMainFunctionRWPeriods_0(void);
void Can_43_FLEXCAN_MainFunction_Read_CanMainFunctionRWPeriods_1(void);
// etc.&lt;/LI-CODE&gt;
&lt;P&gt;But you also need to have the RWperiod respective to the CAN instance correctly configured in the CanHardwareObject container, otherwise, when generating the code, the RWPeriods_0/1/2/3 will not generate:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_2-1753122323908.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/348607i974EAAB5F1F72BAF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_2-1753122323908.png" alt="Julin_AragnM_2-1753122323908.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Julin_AragnM_2-1753122323908.png&lt;/span&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_3-1753122328501.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/348608iB548F35F99DFA7D5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_3-1753122328501.png" alt="Julin_AragnM_3-1753122328501.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Julin_AragnM_3-1753122328501.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_4-1753122358711.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/348609i9387600CFFF1C518/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_4-1753122358711.png" alt="Julin_AragnM_4-1753122358711.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Julin_AragnM_4-1753122358711.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jul 2025 18:26:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-receive/m-p/2137654#M51158</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-07-21T18:26:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 CAN receive</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-receive/m-p/2139386#M51257</link>
      <description>&lt;P&gt;Hi Julián&lt;/P&gt;&lt;P&gt;I had the same settings but with different results.&lt;BR /&gt;The RWPeriods_0/1/2 could not be generated.&lt;BR /&gt;Attached is a screenshot of the setup screen.&lt;/P&gt;&lt;P&gt;I also attach the S32K project under development.&lt;BR /&gt;Please check “AGV_CTRL.mex”.&lt;BR /&gt;The user program has been deleted.&lt;BR /&gt;The version of S32K Design Studio for S32 Platform is “Verison 3.5”.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;toru88&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jul 2025 12:09:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-receive/m-p/2139386#M51257</guid>
      <dc:creator>toru88</dc:creator>
      <dc:date>2025-07-23T12:09:43Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 CAN receive</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-receive/m-p/2141118#M51347</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/173294"&gt;@toru88&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You are right. I tested your project and the correct definitions for the main function RW periods are not being generated. However, this issue seems to be fixed in version 6.0.0 (RTD package I am currently using). Are you able to update the RTD to the newer versions?&lt;/P&gt;
&lt;P&gt;If not, you can simply edit the &lt;STRONG&gt;Can_43_FLEXCAN_Cfg.h&lt;/STRONG&gt; file like below.&lt;/P&gt;
&lt;P&gt;From this:&lt;/P&gt;
&lt;LI-CODE lang="c"&gt;/**
*   @brief      Period for cyclic call of Main Function Read/Write
*/
#define CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_0    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_1    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_2    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_3    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_4    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_5    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_MULTIPLE_WRITE    (STD_ON)
#define CAN_43_FLEXCAN_MAINFUNCTION_MULTIPLE_READ    (STD_ON)&lt;/LI-CODE&gt;
&lt;P&gt;To this:&lt;/P&gt;
&lt;LI-CODE lang="c"&gt;/**
*   @brief      Period for cyclic call of Main Function Read/Write
*/
#define CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_CanMainFunctionRWPeriods_0    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_CanMainFunctionRWPeriods_1    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_CanMainFunctionRWPeriods_2    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_CanMainFunctionRWPeriods_3    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_CanMainFunctionRWPeriods_4    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_CanMainFunctionRWPeriods_5    (0.001F)
#define CAN_43_FLEXCAN_MAINFUNCTION_MULTIPLE_WRITE    (STD_ON)
#define CAN_43_FLEXCAN_MAINFUNCTION_MULTIPLE_READ    (STD_ON)&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 25 Jul 2025 22:32:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-receive/m-p/2141118#M51347</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-07-25T22:32:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 CAN receive</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-receive/m-p/2141200#M51357</link>
      <description>&lt;P&gt;Hi Julián&lt;/P&gt;&lt;P&gt;Since the change to Version 6.0 is not possible, I was able to build by doing the following define.&lt;BR /&gt;Is there any problem with this response?&lt;/P&gt;&lt;P&gt;#define CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_CanMainFunctionRWPeriods_0 CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_0&lt;BR /&gt;#define CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_CanMainFunctionRWPeriods_1 CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_1&lt;BR /&gt;#define CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_CanMainFunctionRWPeriods_2 CAN_43_FLEXCAN_MAINFUNCTION_READ_PERIOD_2&lt;BR /&gt;#define CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_CanMainFunctionRWPeriods_3 CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_3&lt;BR /&gt;#define CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_CanMainFunctionRWPeriods_4 CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_4&lt;BR /&gt;#define CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_CanMainFunctionRWPeriods_5 CAN_43_FLEXCAN_MAINFUNCTION_WRITE_PERIOD_5&lt;/P&gt;&lt;P&gt;I am trying to get it to work, but I cannot send/receive CAN.&lt;BR /&gt;I am setting it up with reference to “Can_Example_S32K344”.&lt;BR /&gt;I think that if I uncheck “Can Loop Back Mode”, I can send/receive CAN data from outside.&lt;BR /&gt;CAN data is received up to the terminal of MCU.&lt;BR /&gt;Is there any sample code to send and receive frames on the CAN bus?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;toru88&lt;/P&gt;</description>
      <pubDate>Sat, 26 Jul 2025 11:42:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-receive/m-p/2141200#M51357</guid>
      <dc:creator>toru88</dc:creator>
      <dc:date>2025-07-26T11:42:00Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 CAN receive</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-receive/m-p/2142070#M51396</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/173294"&gt;@toru88&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;There should be no problem. For transmission, please confirm if baud rate and sampling point are set correctly. Are you using two boards, or a CAN analyzer tool?&lt;/P&gt;
&lt;P&gt;There are some CAN example in community, please refer to them:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/RTD600-MCAL-amp-IP-S32K3X4EVB-T172-FlexCAN-Example-Interrupt/ta-p/2142069" target="_blank"&gt;[RTD600 MCAL &amp;amp; IP] S32K3X4EVB-T172 FlexCAN Example Interrupt/Polling - NXP Community&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-DMA-test-S32DS3-5/ta-p/2015832" target="_blank"&gt;Example S32K344 FlexCAN_Ip TX/RX/EnhanceRXFIFO DMA test S32DS3.5 RTD400 - NXP Community&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K358-FlexCAN-TXRX-ISR-S32DS35-RTD400-500/ta-p/1981987" target="_blank"&gt;Example S32K358 FlexCAN TXRX ISR S32DS35 RTD400/500 - NXP Community&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Mon, 28 Jul 2025 22:29:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-receive/m-p/2142070#M51396</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-07-28T22:29:33Z</dc:date>
    </item>
  </channel>
</rss>