<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K311 Peripheral Configuration Examples (ADC, UART, PWM, I2C, SPI)</title>
    <link>https://community.nxp.com/t5/S32K/S32K311-Peripheral-Configuration-Examples-ADC-UART-PWM-I2C-SPI/m-p/2136258#M51050</link>
    <description>&lt;P&gt;Hello NXP Team,&lt;/P&gt;&lt;P&gt;I am working with the S32K311 microcontroller using S32 Design Studio 3.6.1, and I prefer working at the driver level (bare-metal) instead of using MCAL.&lt;/P&gt;&lt;P&gt;I would like to request example projects, reference code, or documentation to help me configure the following peripherals:&lt;/P&gt;&lt;P&gt;ADC – Single channel configuration with polling or interrupt method&lt;/P&gt;&lt;P&gt;UART – Initialization with basic transmit and receive functions&lt;/P&gt;&lt;P&gt;PWM – Using eMIOS in OPWMB or OPWFMB mode&lt;/P&gt;&lt;P&gt;GPIO – Basic input/output toggling&lt;/P&gt;&lt;P&gt;Startup code – Bare-metal initialization (clock setup, watchdog, etc.)&lt;/P&gt;&lt;P&gt;I am using the S32K311 100HDFP package, and I have the RTD 2.0.0 and 2.0.3 installed.&lt;/P&gt;&lt;P&gt;Please let me know where I can find these examples (SDK paths or GitHub), or share any available application notes or starter projects for S32K311.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Fri, 18 Jul 2025 05:52:31 GMT</pubDate>
    <dc:creator>Kaushal9511</dc:creator>
    <dc:date>2025-07-18T05:52:31Z</dc:date>
    <item>
      <title>S32K311 Peripheral Configuration Examples (ADC, UART, PWM, I2C, SPI)</title>
      <link>https://community.nxp.com/t5/S32K/S32K311-Peripheral-Configuration-Examples-ADC-UART-PWM-I2C-SPI/m-p/2136258#M51050</link>
      <description>&lt;P&gt;Hello NXP Team,&lt;/P&gt;&lt;P&gt;I am working with the S32K311 microcontroller using S32 Design Studio 3.6.1, and I prefer working at the driver level (bare-metal) instead of using MCAL.&lt;/P&gt;&lt;P&gt;I would like to request example projects, reference code, or documentation to help me configure the following peripherals:&lt;/P&gt;&lt;P&gt;ADC – Single channel configuration with polling or interrupt method&lt;/P&gt;&lt;P&gt;UART – Initialization with basic transmit and receive functions&lt;/P&gt;&lt;P&gt;PWM – Using eMIOS in OPWMB or OPWFMB mode&lt;/P&gt;&lt;P&gt;GPIO – Basic input/output toggling&lt;/P&gt;&lt;P&gt;Startup code – Bare-metal initialization (clock setup, watchdog, etc.)&lt;/P&gt;&lt;P&gt;I am using the S32K311 100HDFP package, and I have the RTD 2.0.0 and 2.0.3 installed.&lt;/P&gt;&lt;P&gt;Please let me know where I can find these examples (SDK paths or GitHub), or share any available application notes or starter projects for S32K311.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Fri, 18 Jul 2025 05:52:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K311-Peripheral-Configuration-Examples-ADC-UART-PWM-I2C-SPI/m-p/2136258#M51050</guid>
      <dc:creator>Kaushal9511</dc:creator>
      <dc:date>2025-07-18T05:52:31Z</dc:date>
    </item>
    <item>
      <title>Re: S32K311 Peripheral Configuration Examples (ADC, UART, PWM, I2C, SPI)</title>
      <link>https://community.nxp.com/t5/S32K/S32K311-Peripheral-Configuration-Examples-ADC-UART-PWM-I2C-SPI/m-p/2136455#M51079</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You can find some here, but I do see if they are pure bare metal, I expect they are based on RTD.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/All-Example-S32K311-DS3-5-RTD-3-0-0/ta-p/1841267" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/All-Example-S32K311-DS3-5-RTD-3-0-0/ta-p/1841267&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I have some internal examples for S32K3xx which I can share, but not via community.&lt;/P&gt;
&lt;P&gt;If you like to get those please rise a ticket at NXP.com&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Jul 2025 09:22:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K311-Peripheral-Configuration-Examples-ADC-UART-PWM-I2C-SPI/m-p/2136455#M51079</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2025-07-18T09:22:54Z</dc:date>
    </item>
  </channel>
</rss>