<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K344 CAN FD MCAL in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-CAN-FD-MCAL/m-p/2135577#M51000</link>
    <description>&lt;P&gt;Hi, NXP.&lt;/P&gt;&lt;P&gt;EVB: S32K344&lt;/P&gt;&lt;P&gt;Environment: S32DS RTD 5.0.0&lt;/P&gt;&lt;P&gt;I am building the CAN FD project using MCAL.&lt;/P&gt;&lt;P&gt;Is there any sample project i can refer to?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 17 Jul 2025 07:53:19 GMT</pubDate>
    <dc:creator>IanHsueh</dc:creator>
    <dc:date>2025-07-17T07:53:19Z</dc:date>
    <item>
      <title>S32K344 CAN FD MCAL</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-FD-MCAL/m-p/2135577#M51000</link>
      <description>&lt;P&gt;Hi, NXP.&lt;/P&gt;&lt;P&gt;EVB: S32K344&lt;/P&gt;&lt;P&gt;Environment: S32DS RTD 5.0.0&lt;/P&gt;&lt;P&gt;I am building the CAN FD project using MCAL.&lt;/P&gt;&lt;P&gt;Is there any sample project i can refer to?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jul 2025 07:53:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-FD-MCAL/m-p/2135577#M51000</guid>
      <dc:creator>IanHsueh</dc:creator>
      <dc:date>2025-07-17T07:53:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 CAN FD MCAL</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-FD-MCAL/m-p/2136051#M51027</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247348"&gt;@IanHsueh&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;You can refer to the examples in the RTD. They are the same as shown in this training presentation:&amp;nbsp;&lt;A href="https://www.google.com/url?sa=t&amp;amp;rct=j&amp;amp;q=&amp;amp;esrc=s&amp;amp;source=web&amp;amp;cd=&amp;amp;ved=2ahUKEwixvers5cSOAxUPLtAFHak4DXoQFnoECBgQAQ&amp;amp;url=https%3A%2F%2Fcommunity.nxp.com%2Fpwmxy87654%2Fattachments%2Fpwmxy87654%2FS32K%2F44963%2F2%2FS32K3_RTD_Training_CAN%2520(2).pdf&amp;amp;usg=AOvVaw0WaRiQYlS2l7p6VQ5iRDID&amp;amp;opi=89978449" target="_self"&gt;S32K3XX COMMUNICATION MODULES: FLEXCAN WITH RTD AND LOW-LEVEL DRIVERS.&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;These projects are configured for loopback, so you will need to enable normal/user mode and initialize the transceiver output pins (CAN_H &amp;amp; CAN_L).&lt;/P&gt;
&lt;P&gt;There are also some community posts with examples:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-DMA-test-S32DS3-5/ta-p/2015832" target="_blank"&gt;Example S32K344 FlexCAN_Ip TX/RX/EnhanceRXFIFO DMA test S32DS3.5 RTD400 - NXP Community&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K344-EVB-With-MCAL-FLEXCAN-TJA1153/td-p/1540687" target="_blank"&gt;Solved: S32K344 EVB With MCAL FLEXCAN TJA1153 - NXP Community&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jul 2025 21:29:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-FD-MCAL/m-p/2136051#M51027</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-07-17T21:29:08Z</dc:date>
    </item>
  </channel>
</rss>