<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LIN Wakeup and Timeout in S32K</title>
    <link>https://community.nxp.com/t5/S32K/LIN-Wakeup-and-Timeout/m-p/2134874#M50974</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;BR /&gt;I am using S32k310 with LIN_STACK_2.0.5_D2410_DesignStudio_updatesite and RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite.&lt;BR /&gt;1) I am facing issue when master node send Wake up command, Slave node detect Linnode state as wake up signal but I need to call&amp;nbsp;&lt;SPAN&gt;Lin_43_LPUART_FLEXIO_Wakeup function when&amp;nbsp;LPUART_LIN_IP_RX_ACTIVE_EDGE_DETECT. Could you please describe how LIN Wakeup functionality handle in Lin Stack?&lt;BR /&gt;&lt;/SPAN&gt;2) I want to know more details about LIN Timeout. How LIN Bus will wake up after LIN goes in Sleep mode after timeout?&lt;/P&gt;</description>
    <pubDate>Wed, 16 Jul 2025 09:35:30 GMT</pubDate>
    <dc:creator>pchavapr4</dc:creator>
    <dc:date>2025-07-16T09:35:30Z</dc:date>
    <item>
      <title>LIN Wakeup and Timeout</title>
      <link>https://community.nxp.com/t5/S32K/LIN-Wakeup-and-Timeout/m-p/2134874#M50974</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;BR /&gt;I am using S32k310 with LIN_STACK_2.0.5_D2410_DesignStudio_updatesite and RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite.&lt;BR /&gt;1) I am facing issue when master node send Wake up command, Slave node detect Linnode state as wake up signal but I need to call&amp;nbsp;&lt;SPAN&gt;Lin_43_LPUART_FLEXIO_Wakeup function when&amp;nbsp;LPUART_LIN_IP_RX_ACTIVE_EDGE_DETECT. Could you please describe how LIN Wakeup functionality handle in Lin Stack?&lt;BR /&gt;&lt;/SPAN&gt;2) I want to know more details about LIN Timeout. How LIN Bus will wake up after LIN goes in Sleep mode after timeout?&lt;/P&gt;</description>
      <pubDate>Wed, 16 Jul 2025 09:35:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LIN-Wakeup-and-Timeout/m-p/2134874#M50974</guid>
      <dc:creator>pchavapr4</dc:creator>
      <dc:date>2025-07-16T09:35:30Z</dc:date>
    </item>
    <item>
      <title>Re: LIN Wakeup and Timeout</title>
      <link>https://community.nxp.com/t5/S32K/LIN-Wakeup-and-Timeout/m-p/2135883#M51020</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252753"&gt;@pchavapr4&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I just tested it on the S32K1xx series which I happen to have on bench, my test project can be found here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K144-LIN-Go-to-Sleep/ta-p/2136890" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K144-LIN-Go-to-Sleep/ta-p/2136890&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;It is the same on the S32K310.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can check these functions:&lt;/P&gt;
&lt;P&gt;Lpuart_Lin_Ip_IRQHandlerWhenInitializedExceptBreakIRQ()&lt;/P&gt;
&lt;P&gt;Lpuart_Lin_Ip_ProcessWakeupDetect()&lt;/P&gt;
&lt;P&gt;Lpuart_Lin_Ip_CheckWakeupSignal().&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Sun, 20 Jul 2025 19:55:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LIN-Wakeup-and-Timeout/m-p/2135883#M51020</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-07-20T19:55:15Z</dc:date>
    </item>
  </channel>
</rss>