<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: AD detection is not allowed</title>
    <link>https://community.nxp.com/t5/S32K/AD-detection-is-not-allowed/m-p/942853#M5092</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/ywjack@126.com"&gt;ywjack@126.com&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Is the ADC module calibrated?&lt;/P&gt;&lt;P&gt;Do you use an EVB or your custom board?&lt;/P&gt;&lt;P&gt;Please measure VREFH, VREFL voltage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Aug 2019 12:07:45 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2019-08-05T12:07:45Z</dc:date>
    <item>
      <title>AD detection is not allowed</title>
      <link>https://community.nxp.com/t5/S32K/AD-detection-is-not-allowed/m-p/942852#M5091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The accuracy of the ADC is not accurate. I used the ADC0 channel 13 (PTC15) to detect the voltage. But I found that the 3.3V is the ADC value is 1023, (ten-bit resolution), but I detected 2.5V is the ADC value of 808, already The 0.1V is worse. What's even more strange is that the ADC value I detected for 0.5V is 78. This variation is already very large. Can help me check if my location problem or other problem, I will attach my code configuration&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Aug 2019 02:06:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/AD-detection-is-not-allowed/m-p/942852#M5091</guid>
      <dc:creator>ywjack</dc:creator>
      <dc:date>2019-08-02T02:06:47Z</dc:date>
    </item>
    <item>
      <title>Re: AD detection is not allowed</title>
      <link>https://community.nxp.com/t5/S32K/AD-detection-is-not-allowed/m-p/942853#M5092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/ywjack@126.com"&gt;ywjack@126.com&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Is the ADC module calibrated?&lt;/P&gt;&lt;P&gt;Do you use an EVB or your custom board?&lt;/P&gt;&lt;P&gt;Please measure VREFH, VREFL voltage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Aug 2019 12:07:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/AD-detection-is-not-allowed/m-p/942853#M5092</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-08-05T12:07:45Z</dc:date>
    </item>
  </channel>
</rss>