<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 s32k388 Clock_Ip_Init problem</title>
    <link>https://community.nxp.com/t5/S32K/s32k388-Clock-Ip-Init-problem/m-p/2132515#M50834</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to set the clocks on the s32k388 with the Clock_Ip interface. When generating the default clock configuration in the mex-file, it is not possible to initialise the clocks with the "Clock_Ip_Init" function. This function ends in a Hardfault.&amp;nbsp; Could this be a problem in the SDK, because the default configuration should work without any changes.&lt;BR /&gt;If the Clock_Ip_Init is not called the code is running, but with some slow clock configurations.&lt;/P&gt;&lt;P&gt;Is this problem known or knows somebody a way to set the clocks to specific frequencies?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Used Software:&lt;/P&gt;&lt;P&gt;S32 Design Studio 3.6.2&lt;/P&gt;&lt;P&gt;S32K3XX Real-Time Drivers AUTOSAR R21-11 Version 6.0.0&lt;/P&gt;&lt;P&gt;PlatformSDK_S32K3_S32K388_M7_0_0_LS v 6.0.0&lt;/P&gt;</description>
    <pubDate>Fri, 11 Jul 2025 12:04:59 GMT</pubDate>
    <dc:creator>waldluis</dc:creator>
    <dc:date>2025-07-11T12:04:59Z</dc:date>
    <item>
      <title>s32k388 Clock_Ip_Init problem</title>
      <link>https://community.nxp.com/t5/S32K/s32k388-Clock-Ip-Init-problem/m-p/2132515#M50834</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to set the clocks on the s32k388 with the Clock_Ip interface. When generating the default clock configuration in the mex-file, it is not possible to initialise the clocks with the "Clock_Ip_Init" function. This function ends in a Hardfault.&amp;nbsp; Could this be a problem in the SDK, because the default configuration should work without any changes.&lt;BR /&gt;If the Clock_Ip_Init is not called the code is running, but with some slow clock configurations.&lt;/P&gt;&lt;P&gt;Is this problem known or knows somebody a way to set the clocks to specific frequencies?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Used Software:&lt;/P&gt;&lt;P&gt;S32 Design Studio 3.6.2&lt;/P&gt;&lt;P&gt;S32K3XX Real-Time Drivers AUTOSAR R21-11 Version 6.0.0&lt;/P&gt;&lt;P&gt;PlatformSDK_S32K3_S32K388_M7_0_0_LS v 6.0.0&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jul 2025 12:04:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k388-Clock-Ip-Init-problem/m-p/2132515#M50834</guid>
      <dc:creator>waldluis</dc:creator>
      <dc:date>2025-07-11T12:04:59Z</dc:date>
    </item>
    <item>
      <title>Re: s32k388 Clock_Ip_Init problem</title>
      <link>https://community.nxp.com/t5/S32K/s32k388-Clock-Ip-Init-problem/m-p/2132701#M50850</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/250449"&gt;@waldluis&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I tested a project built from scratch on the S32K388EVB-Q289 using the default clock configuration. I only called the Clock_Ip_Init() function in main(), and did not enter a HardFault. This suggests that the issue is not related to the software or clock configuration.&lt;/P&gt;
&lt;P&gt;If you are working with a custom board, a possible root cause could be hardware-related. Could you please verify the hardware setup?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jul 2025 21:49:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k388-Clock-Ip-Init-problem/m-p/2132701#M50850</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2025-07-11T21:49:07Z</dc:date>
    </item>
    <item>
      <title>Re: s32k388 Clock_Ip_Init problem</title>
      <link>https://community.nxp.com/t5/S32K/s32k388-Clock-Ip-Init-problem/m-p/2133234#M50874</link>
      <description>&lt;P&gt;Hi VaneB,&lt;/P&gt;&lt;P&gt;thanks for the quick response.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes the problem was related to a faster clock source on the custom board. I found that already out in the mean time, but your hint was absolutely right.&lt;/P&gt;&lt;P&gt;After changing to the correct external source input, the clock init is working.&lt;/P&gt;&lt;P&gt;Luis&lt;/P&gt;</description>
      <pubDate>Mon, 14 Jul 2025 09:27:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k388-Clock-Ip-Init-problem/m-p/2133234#M50874</guid>
      <dc:creator>waldluis</dc:creator>
      <dc:date>2025-07-14T09:27:59Z</dc:date>
    </item>
  </channel>
</rss>