<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Issue with IPCF-(S32k358) Initialization on Power Cycle (Dual-Core Setup) in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2131813#M50793</link>
    <description>also tried clearing the shared memory using memset on the IPCF configured addresses like this:&lt;BR /&gt;&lt;BR /&gt;memset((void *)ipcf_shm_instances_cfg.shm_cfg[0].local_shm_addr, 0, (size_t)ipcf_shm_instances_cfg.shm_cfg[0].shm_size);&lt;BR /&gt;memset((void *)ipcf_shm_instances_cfg.shm_cfg[0].remote_shm_addr, 0, (size_t)ipcf_shm_instances_cfg.shm_cfg[0].shm_size);&lt;BR /&gt;&lt;BR /&gt;But unfortunately, that didn’t resolve the issue either.</description>
    <pubDate>Thu, 10 Jul 2025 15:56:11 GMT</pubDate>
    <dc:creator>GaneshBhagwat</dc:creator>
    <dc:date>2025-07-10T15:56:11Z</dc:date>
    <item>
      <title>Issue with IPCF-(S32k358) Initialization on Power Cycle (Dual-Core Setup)</title>
      <link>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2131629#M50776</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Issue with IPCF Initialization on Power Cycle (Dual-Core Setup)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am using &lt;/SPAN&gt;&lt;STRONG&gt;IPCF&lt;/STRONG&gt;&lt;SPAN&gt; to share memory between the two cores. For basic validation, I have two functionalities running:&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;Core 0&lt;/STRONG&gt;: LED Blinking&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Core 2&lt;/STRONG&gt;: PWM generation via &lt;STRONG&gt;eMIOS&lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN&gt;Both cores are configured to run IPCF correctly. When I run the system in &lt;/SPAN&gt;&lt;STRONG&gt;debug mode&lt;/STRONG&gt;&lt;SPAN&gt;, everything works as expected — LED blinking and PWM both function properly. However, when I perform a &lt;/SPAN&gt;&lt;STRONG&gt;power cycle&lt;/STRONG&gt;&lt;SPAN&gt; (turn the board off and on), nothing executes — neither the LED blinks nor the PWM works.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Here’s what I have tried so far:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;Added a delay in Core 2 to avoid any race condition during IPCF initialization.&lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;Tested the system without IPCF&lt;/STRONG&gt;: After removing IPCF, everything works fine, even after a power cycle and in debug mode. This confirms that IPCF is related to the issue.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Narrowed down the issue to this line:&lt;BR /&gt;ipc_shm_init(&amp;amp;ipcf_shm_instances_cfg);&lt;BR /&gt;&lt;BR /&gt;Anything placed after this function call does not execute on a power cycle.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;Tried clearing shared memory before use, suspecting residual data might be causing the problem. However, when I include memory clearing, the system again fails to work after power-up (though it still works in debug mode).&lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here’s how I clear the shared memory:&lt;/P&gt;&lt;P&gt;#define IPCF_LOCAL_MEM_ADDR&amp;nbsp;&amp;nbsp; ((void *)0x20480000U)&lt;BR /&gt;#define IPCF_REMOTE_MEM_ADDR&amp;nbsp; ((void *)0x20482000U)&lt;BR /&gt;#define IPCF_MEM_SIZE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (0x2000U)&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;void clear_ipcf_shared_memory(void)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; memset(IPCF_LOCAL_MEM_ADDR, 0, IPCF_MEM_SIZE);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; memset(IPCF_REMOTE_MEM_ADDR, 0, IPCF_MEM_SIZE);&lt;BR /&gt;}&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;Can you please help me resolve this issue? I have also shared the working project files for reference.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Ganesh Bhagwat&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jul 2025 10:10:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2131629#M50776</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2025-07-10T10:10:39Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with IPCF-(S32k358) Initialization on Power Cycle (Dual-Core Setup)</title>
      <link>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2131813#M50793</link>
      <description>also tried clearing the shared memory using memset on the IPCF configured addresses like this:&lt;BR /&gt;&lt;BR /&gt;memset((void *)ipcf_shm_instances_cfg.shm_cfg[0].local_shm_addr, 0, (size_t)ipcf_shm_instances_cfg.shm_cfg[0].shm_size);&lt;BR /&gt;memset((void *)ipcf_shm_instances_cfg.shm_cfg[0].remote_shm_addr, 0, (size_t)ipcf_shm_instances_cfg.shm_cfg[0].shm_size);&lt;BR /&gt;&lt;BR /&gt;But unfortunately, that didn’t resolve the issue either.</description>
      <pubDate>Thu, 10 Jul 2025 15:56:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2131813#M50793</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2025-07-10T15:56:11Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with IPCF-(S32k358) Initialization on Power Cycle (Dual-Core Setup)</title>
      <link>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2132414#M50823</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244803"&gt;@GaneshBhagwat&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;When you attach the debugger back (without reset), is it stuck in a look in&amp;nbsp;ipc_shm_init() or is there a fault exception?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jul 2025 09:11:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2132414#M50823</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-07-11T09:11:22Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with IPCF-(S32k358) Initialization on Power Cycle (Dual-Core Setup)</title>
      <link>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2132471#M50828</link>
      <description>&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;Thank you for your quick response.&lt;/P&gt;&lt;P&gt;I checked again as you suggested. When I reattach the debugger without a reset, the code goes into a &lt;STRONG&gt;HardFault&lt;/STRONG&gt; inside the function void clear_ipcf_shared_memory(void).&lt;/P&gt;&lt;P&gt;However, if I comment out the call to clear_ipcf_shared_memory(), it still results in a &lt;STRONG&gt;HardFault&lt;/STRONG&gt;, this time inside ipc_shm_init().&lt;/P&gt;&lt;P&gt;I have attached screenshots of both HardFault scenarios for your reference.&lt;BR /&gt;Could you please help me understand what might be causing these faults and guide me on how to resolve the issue?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Ganesh Bhagwat&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jul 2025 10:22:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2132471#M50828</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2025-07-11T10:22:47Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with IPCF-(S32k358) Initialization on Power Cycle (Dual-Core Setup)</title>
      <link>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2132505#M50833</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244803"&gt;@GaneshBhagwat&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;It’s possible that the issue is caused by uninitialized SRAM ECC.&lt;/P&gt;
&lt;P&gt;Typically, SRAM ECC is initialized by the debugger. If the debugger is not used, the application must handle ECC initialization in the startup code. Failing to do so can lead to ECC faults when accessing uninitialized memory.&lt;/P&gt;
&lt;P&gt;To verify this, try checking the memory at address 0x20482008 (BFAR value of the precise bus fault) in the memory view.&amp;nbsp;Do you see ?? at that address?&lt;BR /&gt;If so, it likely indicates an ECC fault due to uninitialized memory.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jul 2025 11:41:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2132505#M50833</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-07-11T11:41:00Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with IPCF-(S32k358) Initialization on Power Cycle (Dual-Core Setup)</title>
      <link>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2132552#M50840</link>
      <description>&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;Thanks again for your quick response.&lt;/P&gt;&lt;P&gt;I've attached the memory view screenshots for your reference—one taken right after starting the debugger, and another captured after a power cycle when the HardFault occurs. The address 0x20482008 does &lt;STRONG&gt;not&lt;/STRONG&gt; show ??, but I noticed that the values at this location are &lt;STRONG&gt;different&lt;/STRONG&gt; between the debugger session and after the power cycle.&lt;/P&gt;&lt;P&gt;Thanks again for your continued support.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Ganesh Bhagwat&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jul 2025 13:36:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2132552#M50840</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2025-07-11T13:36:34Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with IPCF-(S32k358) Initialization on Power Cycle (Dual-Core Setup)</title>
      <link>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2132582#M50842</link>
      <description>Could you please let me know where I can find detailed documentation or examples on how to implement ECC initialization correctly in the startup code?&lt;BR /&gt;&lt;BR /&gt;Also, besides ECC-related issues, are there any other common causes that could lead to similar HardFaults after a power cycle?</description>
      <pubDate>Fri, 11 Jul 2025 14:44:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2132582#M50842</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2025-07-11T14:44:17Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with IPCF-(S32k358) Initialization on Power Cycle (Dual-Core Setup)</title>
      <link>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2134132#M50921</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244803"&gt;@GaneshBhagwat&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Regarding documentation of SRAM ECC, there is just the S32K3xx reference manual and this&amp;nbsp;AN13388:&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN13388" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=AN13388&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;However, you can refer to any RTD example project.&lt;/P&gt;
&lt;P&gt;The SRAM ECC is initialized in the startup code.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1752577890061.png" style="width: 534px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/347633i596A4023180F156E/image-dimensions/534x326?v=v2" width="534" height="326" role="button" title="danielmartynek_0-1752577890061.png" alt="danielmartynek_0-1752577890061.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1752577890061.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;H6&gt;Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.&lt;/H6&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Jul 2025 11:19:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2134132#M50921</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-07-15T11:19:50Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with IPCF-(S32k358) Initialization on Power Cycle (Dual-Core Setup)</title>
      <link>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2134931#M50975</link>
      <description>&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;Thank you for your guidance. Upon further investigation, I discovered that the &lt;STRONG&gt;startup_cm7.s&lt;/STRONG&gt; file includes a section for initializing the shared memory, but it is conditionally compiled under &lt;STRONG&gt;#if defined(MULTIPLE_CORE) &amp;amp;&amp;amp; defined(MULTIPLE_IMAGE)&lt;/STRONG&gt;. By updating the assembler preprocessors to include these definitions, I was able to resolve the issue, and the IPCF initialization now works correctly even after a power cycle. Please see the attached images for reference.&lt;/P&gt;&lt;P&gt;I appreciate your assistance!&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Ganesh Bhagwat&lt;/P&gt;</description>
      <pubDate>Wed, 16 Jul 2025 10:34:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Issue-with-IPCF-S32k358-Initialization-on-Power-Cycle-Dual-Core/m-p/2134931#M50975</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2025-07-16T10:34:32Z</dc:date>
    </item>
  </channel>
</rss>