<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックLogging Lin data using s32k144 and Tja1020  driver</title>
    <link>https://community.nxp.com/t5/S32K/Logging-Lin-data-using-s32k144-and-Tja1020-driver/m-p/2131678#M50785</link>
    <description>&lt;P&gt;Hello everyboby...&lt;/P&gt;&lt;P&gt;I am woking with a project using S32k144 and tja1020 lin driver. I can use the hardware as master or slave for simulating data on lin bus. My problem is i can find any way for logging Lin data on Lin buss, if there are both real master and slave nodes on bus.&lt;/P&gt;&lt;P&gt;With flexcan, we have Listen-only mode for this case, but as i know, there is no mode like this for Lin driver. So could any body have solution for this case? Thankyou very much at all...&lt;/P&gt;</description>
    <pubDate>Thu, 10 Jul 2025 11:42:23 GMT</pubDate>
    <dc:creator>vcuongnv91</dc:creator>
    <dc:date>2025-07-10T11:42:23Z</dc:date>
    <item>
      <title>Logging Lin data using s32k144 and Tja1020  driver</title>
      <link>https://community.nxp.com/t5/S32K/Logging-Lin-data-using-s32k144-and-Tja1020-driver/m-p/2131678#M50785</link>
      <description>&lt;P&gt;Hello everyboby...&lt;/P&gt;&lt;P&gt;I am woking with a project using S32k144 and tja1020 lin driver. I can use the hardware as master or slave for simulating data on lin bus. My problem is i can find any way for logging Lin data on Lin buss, if there are both real master and slave nodes on bus.&lt;/P&gt;&lt;P&gt;With flexcan, we have Listen-only mode for this case, but as i know, there is no mode like this for Lin driver. So could any body have solution for this case? Thankyou very much at all...&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jul 2025 11:42:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Logging-Lin-data-using-s32k144-and-Tja1020-driver/m-p/2131678#M50785</guid>
      <dc:creator>vcuongnv91</dc:creator>
      <dc:date>2025-07-10T11:42:23Z</dc:date>
    </item>
    <item>
      <title>Re: Logging Lin data using s32k144 and Tja1020  driver</title>
      <link>https://community.nxp.com/t5/S32K/Logging-Lin-data-using-s32k144-and-Tja1020-driver/m-p/2131717#M50788</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252537"&gt;@vcuongnv91&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The simplest and most effective solution would be to use a tool like the PEAK-System PLIN-USB. It allows for passive tracing of LIN bus communication without interfering with the signal, making it ideal for debugging and monitoring purposes.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jul 2025 12:56:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Logging-Lin-data-using-s32k144-and-Tja1020-driver/m-p/2131717#M50788</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-07-10T12:56:54Z</dc:date>
    </item>
    <item>
      <title>Re: Logging Lin data using s32k144 and Tja1020  driver</title>
      <link>https://community.nxp.com/t5/S32K/Logging-Lin-data-using-s32k144-and-Tja1020-driver/m-p/2132082#M50804</link>
      <description>Thankyou very much for your quickly reply. With s32k1 / s32k3 and Lin driver like TJA1021 / TJA1124 / SJA1124, is there any solution for logging Lin data like PLin-USB of KEAK-System? Or we must select other hardware for this?</description>
      <pubDate>Fri, 11 Jul 2025 01:40:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Logging-Lin-data-using-s32k144-and-Tja1020-driver/m-p/2132082#M50804</guid>
      <dc:creator>vcuongnv91</dc:creator>
      <dc:date>2025-07-11T01:40:50Z</dc:date>
    </item>
    <item>
      <title>Re: Logging Lin data using s32k144 and Tja1020  driver</title>
      <link>https://community.nxp.com/t5/S32K/Logging-Lin-data-using-s32k144-and-Tja1020-driver/m-p/2132188#M50812</link>
      <description>At this time, my solution is using an other uart channel connect with LpUart-Lin channel for reading data after receiving Header from Lin bus. And it is working fine. Is there any solution better than this?</description>
      <pubDate>Fri, 11 Jul 2025 05:00:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Logging-Lin-data-using-s32k144-and-Tja1020-driver/m-p/2132188#M50812</guid>
      <dc:creator>vcuongnv91</dc:creator>
      <dc:date>2025-07-11T05:00:26Z</dc:date>
    </item>
    <item>
      <title>Re: Logging Lin data using s32k144 and Tja1020  driver</title>
      <link>https://community.nxp.com/t5/S32K/Logging-Lin-data-using-s32k144-and-Tja1020-driver/m-p/2133305#M50884</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252537"&gt;@vcuongnv91&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I think this is the best solution -using another UART module to monitor the RX line from the transceiver.&lt;/P&gt;
&lt;P&gt;Regarding transceivers, there are some devices that have a Listen only modes, for example&amp;nbsp;UJA113X,&amp;nbsp;but this is not the issue here.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/UJA113X_SER.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/UJA113X_SER.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Jul 2025 11:36:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Logging-Lin-data-using-s32k144-and-Tja1020-driver/m-p/2133305#M50884</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-07-14T11:36:32Z</dc:date>
    </item>
  </channel>
</rss>