<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Kのトピックmc33774 balancing not working second time</title>
    <link>https://community.nxp.com/t5/S32K/mc33774-balancing-not-working-second-time/m-p/2130909#M50729</link>
    <description>&lt;P&gt;Hello Forum,&lt;/P&gt;&lt;P&gt;I am currently working on implementing balancing while charging, I use undervoltage based balancing. The first time works great, balancing stops when the cells&amp;nbsp;reach the given voltage (for now sliders on the battery cell emulator)(I check the bal_stat0 register to see if all (8) cells stopped balancing). When i try to balance again after a while (simulating charging), the balancing itself doesnt start anymore, even though i use the same balancing starting function.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a register i need to reset or write to, to allow balancing for a second time?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also use the s32k358 bmu and the bcc_774A driver for the cmu.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Thom&lt;/P&gt;</description>
    <pubDate>Wed, 09 Jul 2025 11:58:27 GMT</pubDate>
    <dc:creator>Thom_H</dc:creator>
    <dc:date>2025-07-09T11:58:27Z</dc:date>
    <item>
      <title>mc33774 balancing not working second time</title>
      <link>https://community.nxp.com/t5/S32K/mc33774-balancing-not-working-second-time/m-p/2130909#M50729</link>
      <description>&lt;P&gt;Hello Forum,&lt;/P&gt;&lt;P&gt;I am currently working on implementing balancing while charging, I use undervoltage based balancing. The first time works great, balancing stops when the cells&amp;nbsp;reach the given voltage (for now sliders on the battery cell emulator)(I check the bal_stat0 register to see if all (8) cells stopped balancing). When i try to balance again after a while (simulating charging), the balancing itself doesnt start anymore, even though i use the same balancing starting function.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a register i need to reset or write to, to allow balancing for a second time?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also use the s32k358 bmu and the bcc_774A driver for the cmu.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Thom&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jul 2025 11:58:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/mc33774-balancing-not-working-second-time/m-p/2130909#M50729</guid>
      <dc:creator>Thom_H</dc:creator>
      <dc:date>2025-07-09T11:58:27Z</dc:date>
    </item>
    <item>
      <title>Re: mc33774 balancing not working second time</title>
      <link>https://community.nxp.com/t5/S32K/mc33774-balancing-not-working-second-time/m-p/2131945#M50798</link>
      <description>&lt;P&gt;Hello Thom_H&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Which measurement mode are you using?, cyclic mode?&lt;/P&gt;
&lt;P&gt;Could you check the BAL_GLOB_CFG and BAL_CH_CFGx registers, are you clearing them after each measurement?&lt;/P&gt;
&lt;P&gt;I recommend you refer to the following community case:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Other-NXP-Products/MC33774-cell-voltage-errors/td-p/2034342" target="_blank"&gt;MC33774 cell voltage errors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;It has useful information and also explains how to access two very useful documents: &lt;STRONG&gt;MC33775A and MC33774A measurement and Errata sheet for MC33774A&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Both are secure documents, so your company must first have an NDA with us.&lt;/P&gt;
&lt;P&gt;I hope this information has helped you, please let me know if you need help with anything else.&lt;/P&gt;
&lt;P&gt;Have a great day and best of luck.&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jul 2025 19:45:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/mc33774-balancing-not-working-second-time/m-p/2131945#M50798</guid>
      <dc:creator>RafaR</dc:creator>
      <dc:date>2025-07-10T19:45:16Z</dc:date>
    </item>
  </channel>
</rss>