<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is there any sample code available for TCP client communication (send/receive) on S32K3 platform in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Is-there-any-sample-code-available-for-TCP-client-communication/m-p/2130066#M50670</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;you can refer to TCP/IP stack demo examples. Download it from&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D" target="_blank"&gt;https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D&lt;/A&gt; and install it along right RTD version in S32DS. See package release note for installation steps.&lt;/P&gt;
&lt;P&gt;The TCP/IP stack features a set of applications, which demonstrates key functionalities of this software product. One of application is the TCP echo server, using either Raw or Netconn API.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Tue, 08 Jul 2025 10:19:15 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2025-07-08T10:19:15Z</dc:date>
    <item>
      <title>Is there any sample code available for TCP client communication (send/receive) on S32K3 platform?</title>
      <link>https://community.nxp.com/t5/S32K/Is-there-any-sample-code-available-for-TCP-client-communication/m-p/2129126#M50610</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Is there any sample code available for TCP client communication (send/receive) on S32K3 platform?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jul 2025 08:03:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-there-any-sample-code-available-for-TCP-client-communication/m-p/2129126#M50610</guid>
      <dc:creator>zhangzhixing</dc:creator>
      <dc:date>2025-07-07T08:03:25Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any sample code available for TCP client communication (send/receive) on S32K3 platform</title>
      <link>https://community.nxp.com/t5/S32K/Is-there-any-sample-code-available-for-TCP-client-communication/m-p/2130066#M50670</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;you can refer to TCP/IP stack demo examples. Download it from&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D" target="_blank"&gt;https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D&lt;/A&gt; and install it along right RTD version in S32DS. See package release note for installation steps.&lt;/P&gt;
&lt;P&gt;The TCP/IP stack features a set of applications, which demonstrates key functionalities of this software product. One of application is the TCP echo server, using either Raw or Netconn API.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 08 Jul 2025 10:19:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-there-any-sample-code-available-for-TCP-client-communication/m-p/2130066#M50670</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-07-08T10:19:15Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any sample code available for TCP client communication (send/receive) on S32K3 platform</title>
      <link>https://community.nxp.com/t5/S32K/Is-there-any-sample-code-available-for-TCP-client-communication/m-p/2134873#M50973</link>
      <description>&lt;P&gt;tcp client done !&lt;/P&gt;</description>
      <pubDate>Wed, 16 Jul 2025 09:32:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-there-any-sample-code-available-for-TCP-client-communication/m-p/2134873#M50973</guid>
      <dc:creator>zhangzhixing</dc:creator>
      <dc:date>2025-07-16T09:32:26Z</dc:date>
    </item>
  </channel>
</rss>