<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re:  FreeRTOS 10 for S32K144  in S32K</title>
    <link>https://community.nxp.com/t5/S32K/FreeRTOS-10-for-S32K144/m-p/940944#M5067</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Witold Kowolik&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SDK is not supported in Linux environment, sorry for the inconveniences that this might cause you.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="jive_macro_thread jive_macro" data-orig-content="S32DS and S32K1XX SDK on Linux" href="https://community.nxp.com/message/1115753"&gt;S32DS and S32K1XX SDK on Linux&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Jul 2019 23:49:29 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2019-07-22T23:49:29Z</dc:date>
    <item>
      <title>FreeRTOS 10 for S32K144</title>
      <link>https://community.nxp.com/t5/S32K/FreeRTOS-10-for-S32K144/m-p/940943#M5066</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to write some simple testing application for S32K144 using FreeRTOS 10. I am using S32DS 2018.R1 under Linux. Unfortunately there is something wrong with S32DS under Linux and I cannot select anywhere FreeRTOS in S32DS. I've seen a few tutorials on the net where FreeRTOS can be used from S32DS but I have no such option in my version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thus I'm planning to create FreeRTOS project manually. I guess I need dedicated FreeRTOS for S32K144 so I'd like to ask if there are official FreeRTOS v10 sources for S32K144 published somewhere?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jul 2019 07:55:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FreeRTOS-10-for-S32K144/m-p/940943#M5066</guid>
      <dc:creator>sdrb</dc:creator>
      <dc:date>2019-07-04T07:55:35Z</dc:date>
    </item>
    <item>
      <title>Re:  FreeRTOS 10 for S32K144</title>
      <link>https://community.nxp.com/t5/S32K/FreeRTOS-10-for-S32K144/m-p/940944#M5067</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Witold Kowolik&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SDK is not supported in Linux environment, sorry for the inconveniences that this might cause you.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="jive_macro_thread jive_macro" data-orig-content="S32DS and S32K1XX SDK on Linux" href="https://community.nxp.com/message/1115753"&gt;S32DS and S32K1XX SDK on Linux&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jul 2019 23:49:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FreeRTOS-10-for-S32K144/m-p/940944#M5067</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-07-22T23:49:29Z</dc:date>
    </item>
  </channel>
</rss>