<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K3 register protection or error ditection</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-register-protection-or-error-ditection/m-p/2124307#M50308</link>
    <description>&lt;P&gt;hello.&lt;BR /&gt;I have a question for S32K312 register protection.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Can I periodically check the value of the register settings during operation?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; 1-1. If possible, how to check or an example project would be appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. Among the registers that are set at Init, are there any registers that can be written and changed with arbitrary values?&lt;BR /&gt;Ex) Write and read with specific values (0xAA, 0x55, etc.) to the register area used, and recover the register after checking the physical integrity.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank You.&lt;/P&gt;</description>
    <pubDate>Fri, 27 Jun 2025 00:27:35 GMT</pubDate>
    <dc:creator>Gitae</dc:creator>
    <dc:date>2025-06-27T00:27:35Z</dc:date>
    <item>
      <title>S32K3 register protection or error ditection</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-register-protection-or-error-ditection/m-p/2124307#M50308</link>
      <description>&lt;P&gt;hello.&lt;BR /&gt;I have a question for S32K312 register protection.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Can I periodically check the value of the register settings during operation?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; 1-1. If possible, how to check or an example project would be appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. Among the registers that are set at Init, are there any registers that can be written and changed with arbitrary values?&lt;BR /&gt;Ex) Write and read with specific values (0xAA, 0x55, etc.) to the register area used, and recover the register after checking the physical integrity.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank You.&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jun 2025 00:27:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-register-protection-or-error-ditection/m-p/2124307#M50308</guid>
      <dc:creator>Gitae</dc:creator>
      <dc:date>2025-06-27T00:27:35Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 register protection or error ditection</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-register-protection-or-error-ditection/m-p/2124472#M50314</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;1. Can I periodically check the value of the register settings during operation?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Yes, you can read protected registers with no limitation.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;1-1. If possible, how to check or an example project would be appreciated.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Simply perform read and compare it in your SW with expected values.&lt;/P&gt;
&lt;P&gt;But I see no sense in this, as if there is any access to protected register, exception is called.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;2. Among the registers that are set at Init, are there any registers that can be written and changed with arbitrary values?&lt;BR /&gt;Ex) Write and read with specific values (0xAA, 0x55, etc.) to the register area used, and recover the register after checking the physical integrity.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;You have 2 lock possibilities:&lt;/P&gt;
&lt;P&gt;1. Soft lock - can be unlocked by sequence&lt;/P&gt;
&lt;P&gt;2. Hard lock - unlocked only on power on reset.&lt;/P&gt;
&lt;P&gt;For more details please refer to&amp;nbsp;Chapter 55 Register Protection (REG_PROT) of reference manual.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jun 2025 06:45:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-register-protection-or-error-ditection/m-p/2124472#M50314</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2025-06-27T06:45:57Z</dc:date>
    </item>
  </channel>
</rss>