<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K144_CAN_BUSOFF in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-CAN-BUSOFF/m-p/2122984#M50238</link>
    <description>&lt;P&gt;How can I disable the "CAN BusOff" automatic recovery function and create a "CAN BusOff" mechanism? (Based on SDK 3.0.0)&lt;BR /&gt;When "CAN BusOff" occurs, a fault is reported and ten quick recover attempts are made. If the ten quick recover attempts fail, switch to slow recovery.&lt;/P&gt;&lt;P&gt;Is it necessary to shut down all the Tx tasks when "CAN BusOff" occurs?&lt;/P&gt;</description>
    <pubDate>Wed, 25 Jun 2025 09:01:40 GMT</pubDate>
    <dc:creator>LzdOo</dc:creator>
    <dc:date>2025-06-25T09:01:40Z</dc:date>
    <item>
      <title>S32K144_CAN_BUSOFF</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-CAN-BUSOFF/m-p/2122984#M50238</link>
      <description>&lt;P&gt;How can I disable the "CAN BusOff" automatic recovery function and create a "CAN BusOff" mechanism? (Based on SDK 3.0.0)&lt;BR /&gt;When "CAN BusOff" occurs, a fault is reported and ten quick recover attempts are made. If the ten quick recover attempts fail, switch to slow recovery.&lt;/P&gt;&lt;P&gt;Is it necessary to shut down all the Tx tasks when "CAN BusOff" occurs?&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jun 2025 09:01:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-CAN-BUSOFF/m-p/2122984#M50238</guid>
      <dc:creator>LzdOo</dc:creator>
      <dc:date>2025-06-25T09:01:40Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144_CAN_BUSOFF</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-CAN-BUSOFF/m-p/2123445#M50261</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/250211"&gt;@LzdOo&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please refer to this community post:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/s32K144-can-bus-off/td-p/762743" target="_blank"&gt;s32K144 can bus off - NXP Community.&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Automatic bus off recovery can be disabled by setting the CTRL1[BOFFREC] bit.&amp;nbsp;If the bit is asserted, automatic recovering from Bus Off is disabled and the module remains in Bus Off state until the bit is negated by the user.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Tx tasks should stop once a bus off fault occurs, as per the CAN 2.0 specification; a&amp;nbsp;bus off unit is not allowed to have any influence on the bus (e.g. output drivers switched off).&lt;/P&gt;
&lt;P&gt;You can also refer to this FlexCAN error test example:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-FlexCAN-TX-RX-Error-ISR-test-S32DS2-2/ta-p/1278224" target="_blank"&gt;Example S32K144 FlexCAN TX/RX/Error ISR test S32DS2.2 - NXP Community&lt;/A&gt;. Simply&lt;SPAN&gt;&amp;nbsp;short CANH with GND and send message using either SW1 or SW2, FlexCAN enters bus off (error event) and blue LED is ON.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jun 2025 21:35:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-CAN-BUSOFF/m-p/2123445#M50261</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-06-25T21:35:45Z</dc:date>
    </item>
  </channel>
</rss>