<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックMCAL API Descrption</title>
    <link>https://community.nxp.com/t5/S32K/MCAL-API-Descrption/m-p/2122663#M50218</link>
    <description>&lt;P&gt;Currently, in the MCAL static code, I can only understand the usage of the API through the function comments. I would like to know if there are any documentation or websites available to query the explanations and parameter descriptions of each API in the MCAL API functions?&lt;/P&gt;</description>
    <pubDate>Wed, 25 Jun 2025 02:24:09 GMT</pubDate>
    <dc:creator>Embedded_novice</dc:creator>
    <dc:date>2025-06-25T02:24:09Z</dc:date>
    <item>
      <title>MCAL API Descrption</title>
      <link>https://community.nxp.com/t5/S32K/MCAL-API-Descrption/m-p/2122663#M50218</link>
      <description>&lt;P&gt;Currently, in the MCAL static code, I can only understand the usage of the API through the function comments. I would like to know if there are any documentation or websites available to query the explanations and parameter descriptions of each API in the MCAL API functions?&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jun 2025 02:24:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCAL-API-Descrption/m-p/2122663#M50218</guid>
      <dc:creator>Embedded_novice</dc:creator>
      <dc:date>2025-06-25T02:24:09Z</dc:date>
    </item>
    <item>
      <title>Re: MCAL API Descrption</title>
      <link>https://community.nxp.com/t5/S32K/MCAL-API-Descrption/m-p/2122838#M50224</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;API documentation is present directly at plugins:&lt;/P&gt;
&lt;P&gt;For example ADC:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_0-1750833454808.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/344532i1D784B3B4EFC0AD7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="petervlna_0-1750833454808.png" alt="petervlna_0-1750833454808.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;There is doc folder where you can find implementation and user manual.&lt;/P&gt;
&lt;P&gt;best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jun 2025 06:38:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCAL-API-Descrption/m-p/2122838#M50224</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2025-06-25T06:38:58Z</dc:date>
    </item>
    <item>
      <title>Re: MCAL API Descrption</title>
      <link>https://community.nxp.com/t5/S32K/MCAL-API-Descrption/m-p/2122854#M50227</link>
      <description>However, this seems to only include the outermost encapsulation interface. I was able to find the function Mcu_GetPllStatus, but the deeper-level function implementations within it, such as Mcu_Ipw_GetPllStatus, cannot be found in the manual. Can I understand it as follows: The manual only presents the API of the outermost layer, while the internal implementation API can only be understood through the comments?</description>
      <pubDate>Wed, 25 Jun 2025 06:51:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCAL-API-Descrption/m-p/2122854#M50227</guid>
      <dc:creator>Embedded_novice</dc:creator>
      <dc:date>2025-06-25T06:51:20Z</dc:date>
    </item>
    <item>
      <title>Re: MCAL API Descrption</title>
      <link>https://community.nxp.com/t5/S32K/MCAL-API-Descrption/m-p/2123770#M50278</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You are right. I do not see them in the API documentation.&lt;/P&gt;
&lt;P&gt;Therefore I expect it could part of general AUTOSAR specification.&lt;/P&gt;
&lt;P&gt;But I have only ASR 4.0 documentation here and I did not find it there.&lt;/P&gt;
&lt;P&gt;As you shared, you can understand it from the code c and h files. Seems to me the quickest way to see the parameters.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Thu, 26 Jun 2025 08:10:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCAL-API-Descrption/m-p/2123770#M50278</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2025-06-26T08:10:34Z</dc:date>
    </item>
  </channel>
</rss>