<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K3 SPD in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-SPD/m-p/2122137#M50196</link>
    <description>&lt;P&gt;Hi@&lt;SPAN&gt;Neo1096&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Please follow your duplicated question:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K3-SPD-DMA/td-p/2121214" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K3-SPD-DMA/td-p/2121214&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 24 Jun 2025 10:30:15 GMT</pubDate>
    <dc:creator>Senlent</dc:creator>
    <dc:date>2025-06-24T10:30:15Z</dc:date>
    <item>
      <title>S32K3 SPD</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-SPD/m-p/2121296#M50150</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I use RTD400 and SPD105, and the development board is the S32K312 144P development board&lt;/P&gt;&lt;P&gt;I added the uart module to the tested SPD module (including RAM and flash injection errors) program, and it worked normally. Then I added other modules. (Currently, only the DMA part has been tested, and adding only uart seems to be fine.) Without making any Settings, even if the header file is not referenced in the code, The program will also be in the function Clock_Ip_SetWaitStates(); Then it enters a hardware error interrupt.&lt;/P&gt;&lt;P&gt;I uploaded the code of the FCCU module without adding DMA, and it can run normally. However, after adding it, the clock initialization program hardware error occurs. What could be the reason for this and how can this problem be solved?&lt;/P&gt;</description>
      <pubDate>Mon, 23 Jun 2025 09:05:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-SPD/m-p/2121296#M50150</guid>
      <dc:creator>Neo1096</dc:creator>
      <dc:date>2025-06-23T09:05:03Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 SPD</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-SPD/m-p/2122137#M50196</link>
      <description>&lt;P&gt;Hi@&lt;SPAN&gt;Neo1096&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Please follow your duplicated question:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K3-SPD-DMA/td-p/2121214" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K3-SPD-DMA/td-p/2121214&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Jun 2025 10:30:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-SPD/m-p/2122137#M50196</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2025-06-24T10:30:15Z</dc:date>
    </item>
  </channel>
</rss>