<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: s32k312 I2C Clock Source</title>
    <link>https://community.nxp.com/t5/S32K/s32k312-I2C-Clock-Source/m-p/2119717#M50087</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;It looks similar to the previous question, please refer to the screenshot in that question:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/s32k312-I2C-Clock-Source/m-p/2118956#M50051" target="_self"&gt;s32k312 I2C Clock Source&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Please add &lt;STRONG&gt;Clock_Ip_ReferencePoints&lt;/STRONG&gt;&amp;nbsp;in &lt;STRONG&gt;Peripherals&lt;/STRONG&gt; tool and configure &lt;STRONG&gt;AIPS_SLOW_CLK&lt;/STRONG&gt; as the &lt;STRONG&gt;MODULE_CLK&lt;/STRONG&gt; source of LPI2C.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Thu, 19 Jun 2025 23:29:47 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2025-06-19T23:29:47Z</dc:date>
    <item>
      <title>s32k312 I2C Clock Source</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-I2C-Clock-Source/m-p/2118970#M50052</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I used S32K312 and there is a problem to select I2C Clock Source&lt;/P&gt;&lt;P&gt;Even though i set the clock source to 30Mhz and active, i2c clcok source candidates are not identified when i set i2c peripheral.&lt;/P&gt;&lt;P&gt;candidate group of SPI could selected without any problems, can you help me?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;MCU : S32K312NHT0MPASR&lt;/P&gt;&lt;P&gt;IDE : Design Studio 3.6.2&lt;/P&gt;&lt;P&gt;RTD :&amp;nbsp;S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0 (Latest by current standards)&lt;/P&gt;</description>
      <pubDate>Thu, 19 Jun 2025 02:09:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-I2C-Clock-Source/m-p/2118970#M50052</guid>
      <dc:creator>Hoon</dc:creator>
      <dc:date>2025-06-19T02:09:24Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 I2C Clock Source</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-I2C-Clock-Source/m-p/2119717#M50087</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;It looks similar to the previous question, please refer to the screenshot in that question:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/s32k312-I2C-Clock-Source/m-p/2118956#M50051" target="_self"&gt;s32k312 I2C Clock Source&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Please add &lt;STRONG&gt;Clock_Ip_ReferencePoints&lt;/STRONG&gt;&amp;nbsp;in &lt;STRONG&gt;Peripherals&lt;/STRONG&gt; tool and configure &lt;STRONG&gt;AIPS_SLOW_CLK&lt;/STRONG&gt; as the &lt;STRONG&gt;MODULE_CLK&lt;/STRONG&gt; source of LPI2C.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 19 Jun 2025 23:29:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-I2C-Clock-Source/m-p/2119717#M50087</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-06-19T23:29:47Z</dc:date>
    </item>
  </channel>
</rss>