<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 key Management</title>
    <link>https://community.nxp.com/t5/S32K/key-Management/m-p/2118594#M50031</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1.I am working with the S32K314 and have implemented ECDH. During testing, I commented out the key generation code. For production, I would like to ensure that key generation occurs only once and is not repeated on every boot. Is there a recommended approach or any specific flags in the HSE to handle this?&lt;/P&gt;&lt;P&gt;2.Additionally, I currently declare a key as a global variable and write it to NVM. However, this results in the key being visible globally in the code. Is there a way to import the key directly into the HSE without declaring it as a global variable?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 18 Jun 2025 13:24:51 GMT</pubDate>
    <dc:creator>kerti1</dc:creator>
    <dc:date>2025-06-18T13:24:51Z</dc:date>
    <item>
      <title>key Management</title>
      <link>https://community.nxp.com/t5/S32K/key-Management/m-p/2118594#M50031</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1.I am working with the S32K314 and have implemented ECDH. During testing, I commented out the key generation code. For production, I would like to ensure that key generation occurs only once and is not repeated on every boot. Is there a recommended approach or any specific flags in the HSE to handle this?&lt;/P&gt;&lt;P&gt;2.Additionally, I currently declare a key as a global variable and write it to NVM. However, this results in the key being visible globally in the code. Is there a way to import the key directly into the HSE without declaring it as a global variable?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jun 2025 13:24:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/key-Management/m-p/2118594#M50031</guid>
      <dc:creator>kerti1</dc:creator>
      <dc:date>2025-06-18T13:24:51Z</dc:date>
    </item>
    <item>
      <title>Re: key Management</title>
      <link>https://community.nxp.com/t5/S32K/key-Management/m-p/2121155#M50137</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/249628"&gt;@kerti1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. When generating a key, NVM key slot must be empty. The generation will not be successful, if the key was already generated in the slot.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you want to update internally generated key, it can be done via the key import service.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2. There are two options:&lt;/P&gt;
&lt;P&gt;a) Use some communication interface in production to provide the keys for import.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;b) Force the keys to some separate segment in flash memory. Once the keys are imported, erase the memory segment.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Mon, 23 Jun 2025 06:24:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/key-Management/m-p/2121155#M50137</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2025-06-23T06:24:34Z</dc:date>
    </item>
  </channel>
</rss>