<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K1xx D-Flash Configuration in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K1xx-D-Flash-Configuration/m-p/2118372#M50016</link>
    <description>&lt;P&gt;Hello, all&lt;/P&gt;&lt;P&gt;now we have a question, that the S32K1xx Serial MCU, e.g. S32K148, the D-Flash area can be reconfigurat as P-Flash to run code?&lt;/P&gt;&lt;P&gt;can we do this, if yes, how?&lt;/P&gt;&lt;P&gt;Many Thanks and Best Regards&lt;/P&gt;</description>
    <pubDate>Wed, 18 Jun 2025 08:19:00 GMT</pubDate>
    <dc:creator>Kevin74</dc:creator>
    <dc:date>2025-06-18T08:19:00Z</dc:date>
    <item>
      <title>S32K1xx D-Flash Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K1xx-D-Flash-Configuration/m-p/2118372#M50016</link>
      <description>&lt;P&gt;Hello, all&lt;/P&gt;&lt;P&gt;now we have a question, that the S32K1xx Serial MCU, e.g. S32K148, the D-Flash area can be reconfigurat as P-Flash to run code?&lt;/P&gt;&lt;P&gt;can we do this, if yes, how?&lt;/P&gt;&lt;P&gt;Many Thanks and Best Regards&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jun 2025 08:19:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K1xx-D-Flash-Configuration/m-p/2118372#M50016</guid>
      <dc:creator>Kevin74</dc:creator>
      <dc:date>2025-06-18T08:19:00Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1xx D-Flash Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K1xx-D-Flash-Configuration/m-p/2118633#M50032</link>
      <description>&lt;P&gt;Yes, it is possible.&lt;/P&gt;
&lt;P&gt;It is needed to perform flash_partitioning operation according user configuration. Pay attention to AN11983 - Using the S32K1xx EEPROM Functionality:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN11983.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN11983.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;specifically Tables 3 – 5.&lt;/P&gt;
&lt;P&gt;Retention and endurance is the same in this use:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="davidtosenovjan_0-1750256789019.png" style="width: 663px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/343577i3B0E602BD2B8110E/image-dimensions/663x300?v=v2" width="663" height="300" role="button" title="davidtosenovjan_0-1750256789019.png" alt="davidtosenovjan_0-1750256789019.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;davidtosenovjan_0-1750256789019.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jun 2025 14:27:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K1xx-D-Flash-Configuration/m-p/2118633#M50032</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2025-06-18T14:27:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1xx D-Flash Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K1xx-D-Flash-Configuration/m-p/2119941#M50102</link>
      <description>&lt;DIV class=""&gt;&lt;P&gt;Hello davidtosenovja:&lt;/P&gt;&lt;P&gt;Many Thanks! i will check this option.&lt;/P&gt;&lt;P&gt;Best Regards!&lt;/P&gt;&lt;/DIV&gt;</description>
      <pubDate>Fri, 20 Jun 2025 06:47:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K1xx-D-Flash-Configuration/m-p/2119941#M50102</guid>
      <dc:creator>Kevin74</dc:creator>
      <dc:date>2025-06-20T06:47:39Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1xx D-Flash Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K1xx-D-Flash-Configuration/m-p/2121288#M50149</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;But what i mean is whether D-Flash can run as P-Flash, for this need man do some reconfiguration of D-Flash or can man direct store the user program code into D-Flash and run them?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many Thanks and BR&lt;/P&gt;</description>
      <pubDate>Mon, 23 Jun 2025 08:51:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K1xx-D-Flash-Configuration/m-p/2121288#M50149</guid>
      <dc:creator>Kevin74</dc:creator>
      <dc:date>2025-06-23T08:51:17Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1xx D-Flash Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K1xx-D-Flash-Configuration/m-p/2122948#M50233</link>
      <description>&lt;P&gt;Yes, as default configuration is not valid:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="davidtosenovjan_1-1750839269966.png" style="width: 663px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/344577iA69C1818DD2DC0AD/image-dimensions/663x420?v=v2" width="663" height="420" role="button" title="davidtosenovjan_1-1750839269966.png" alt="davidtosenovjan_1-1750839269966.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;davidtosenovjan_1-1750839269966.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Program partition operation is needed to do once per device lifetime, it is not supposed to be done in every startup.&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jun 2025 08:14:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K1xx-D-Flash-Configuration/m-p/2122948#M50233</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2025-06-25T08:14:57Z</dc:date>
    </item>
  </channel>
</rss>