<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Kのトピック#s32k396 sgen</title>
    <link>https://community.nxp.com/t5/S32K/s32k396-sgen/m-p/2118170#M49997</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am currently working with the S32K396 MCU and would like to implement RDC-less functionality using the SGEN peripheral.&lt;/P&gt;&lt;P&gt;I am using the S32 Design Studio and the RTD model for Basic Software configuration.&lt;/P&gt;&lt;P&gt;Assuming that the SGEN is properly configured, I would like to know which peripheral I can use to output the signal generated by SGEN so that I can observe it on an oscilloscope.&lt;/P&gt;&lt;P&gt;Additionally, which MCAL driver(s) should be configured in order to use the SGEN module?&lt;/P&gt;&lt;P&gt;Lastly, is it even possible to output a sine wave generated by SGEN to a physical pin?&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;</description>
    <pubDate>Wed, 18 Jun 2025 02:23:54 GMT</pubDate>
    <dc:creator>maaong</dc:creator>
    <dc:date>2025-06-18T02:23:54Z</dc:date>
    <item>
      <title>#s32k396 sgen</title>
      <link>https://community.nxp.com/t5/S32K/s32k396-sgen/m-p/2118170#M49997</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am currently working with the S32K396 MCU and would like to implement RDC-less functionality using the SGEN peripheral.&lt;/P&gt;&lt;P&gt;I am using the S32 Design Studio and the RTD model for Basic Software configuration.&lt;/P&gt;&lt;P&gt;Assuming that the SGEN is properly configured, I would like to know which peripheral I can use to output the signal generated by SGEN so that I can observe it on an oscilloscope.&lt;/P&gt;&lt;P&gt;Additionally, which MCAL driver(s) should be configured in order to use the SGEN module?&lt;/P&gt;&lt;P&gt;Lastly, is it even possible to output a sine wave generated by SGEN to a physical pin?&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jun 2025 02:23:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k396-sgen/m-p/2118170#M49997</guid>
      <dc:creator>maaong</dc:creator>
      <dc:date>2025-06-18T02:23:54Z</dc:date>
    </item>
    <item>
      <title>Re: #s32k396 sgen</title>
      <link>https://community.nxp.com/t5/S32K/s32k396-sgen/m-p/2118387#M50017</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;I am using the S32 Design Studio and the RTD model for Basic Software configuration.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;SGEN is not currently supported by RTD.&lt;/P&gt;
&lt;P&gt;You can use baremetal example code which is on our web for single motor control kit:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/MCSPTR2AK396" target="_blank"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/MCSPTR2AK396&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;There is set HW trigger, but you can modify it according to your needs.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;Lastly, is it even possible to output a sine wave generated by SGEN to a physical pin?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Yes. Refer to IOMUX table attached to reference manual.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_0-1750235715575.png" style="width: 729px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/343508i0D2D8192E48B16ED/image-dimensions/729x237?v=v2" width="729" height="237" role="button" title="petervlna_0-1750235715575.png" alt="petervlna_0-1750235715575.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;petervlna_0-1750235715575.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jun 2025 08:35:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k396-sgen/m-p/2118387#M50017</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2025-06-18T08:35:40Z</dc:date>
    </item>
  </channel>
</rss>