<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32K3 HSE Demo project compile error</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-HSE-Demo-project-compile-error/m-p/2117564#M49964</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;This is an outdated example based on &lt;STRONG&gt;S32K3_RTD_1_0_0_HF01_D2111&lt;/STRONG&gt;. You need to use S32DS.3.4 with &lt;STRONG&gt;S32K3 Real Time Drivers Version 1.0.0 HotFix 01&lt;/STRONG&gt; installed to compile it.&lt;BR /&gt;Considering that you are a Chinese customer, it is recommended to ask Distributor FAE for the latest &lt;STRONG&gt;s32k3_hse_lib_rtd400hf01_20250221.7z&lt;/STRONG&gt; which contains the project for installing HSE FW for S32K312.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Tue, 17 Jun 2025 08:18:42 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2025-06-17T08:18:42Z</dc:date>
    <item>
      <title>S32K3 HSE Demo project compile error</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE-Demo-project-compile-error/m-p/2117440#M49950</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/343241iBBA705BD18A40F6B/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;image.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;After decompressing the official project, there is a compilation error.&lt;/P&gt;&lt;P&gt;How should I do?&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jun 2025 06:02:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE-Demo-project-compile-error/m-p/2117440#M49950</guid>
      <dc:creator>Temple</dc:creator>
      <dc:date>2025-06-17T06:02:34Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 HSE Demo project compile error</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE-Demo-project-compile-error/m-p/2117564#M49964</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;This is an outdated example based on &lt;STRONG&gt;S32K3_RTD_1_0_0_HF01_D2111&lt;/STRONG&gt;. You need to use S32DS.3.4 with &lt;STRONG&gt;S32K3 Real Time Drivers Version 1.0.0 HotFix 01&lt;/STRONG&gt; installed to compile it.&lt;BR /&gt;Considering that you are a Chinese customer, it is recommended to ask Distributor FAE for the latest &lt;STRONG&gt;s32k3_hse_lib_rtd400hf01_20250221.7z&lt;/STRONG&gt; which contains the project for installing HSE FW for S32K312.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jun 2025 08:18:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE-Demo-project-compile-error/m-p/2117564#M49964</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-06-17T08:18:42Z</dc:date>
    </item>
  </channel>
</rss>