<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Cotactor feedack using ADC with SW triggering in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Cotactor-feedack-using-ADC-with-SW-triggering/m-p/2114492#M49810</link>
    <description>&lt;P&gt;hi, I am currently working on contactor feedback through ADC with software triggering but i the ADC is being either in IDLE or BUSY state, Also i am not sure about the complete configuration changes in the adc and related peripherals , due to some configurations i am getting hard fault. although i have added CDD_m3hhb_adc_exernal_access.h/.c file in the build as well as well as the adc related driver files,&amp;nbsp; if any body has any reference or example code do, help&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 11 Jun 2025 13:01:13 GMT</pubDate>
    <dc:creator>Joseph_David</dc:creator>
    <dc:date>2025-06-11T13:01:13Z</dc:date>
    <item>
      <title>Cotactor feedack using ADC with SW triggering</title>
      <link>https://community.nxp.com/t5/S32K/Cotactor-feedack-using-ADC-with-SW-triggering/m-p/2114492#M49810</link>
      <description>&lt;P&gt;hi, I am currently working on contactor feedback through ADC with software triggering but i the ADC is being either in IDLE or BUSY state, Also i am not sure about the complete configuration changes in the adc and related peripherals , due to some configurations i am getting hard fault. although i have added CDD_m3hhb_adc_exernal_access.h/.c file in the build as well as well as the adc related driver files,&amp;nbsp; if any body has any reference or example code do, help&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Jun 2025 13:01:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Cotactor-feedack-using-ADC-with-SW-triggering/m-p/2114492#M49810</guid>
      <dc:creator>Joseph_David</dc:creator>
      <dc:date>2025-06-11T13:01:13Z</dc:date>
    </item>
    <item>
      <title>Re: Cotactor feedack using ADC with SW triggering</title>
      <link>https://community.nxp.com/t5/S32K/Cotactor-feedack-using-ADC-with-SW-triggering/m-p/2114682#M49816</link>
      <description>&lt;P&gt;Thank you for your interest in our products and for contributing to our community.&lt;/P&gt;
&lt;P&gt;Can you tell us which device are you using please?&lt;/P&gt;</description>
      <pubDate>Wed, 11 Jun 2025 18:37:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Cotactor-feedack-using-ADC-with-SW-triggering/m-p/2114682#M49816</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2025-06-11T18:37:30Z</dc:date>
    </item>
    <item>
      <title>Re: Cotactor feedack using ADC with SW triggering</title>
      <link>https://community.nxp.com/t5/S32K/Cotactor-feedack-using-ADC-with-SW-triggering/m-p/2115142#M49837</link>
      <description>S32k358 microcontroller and LiFePO4 battery pack</description>
      <pubDate>Thu, 12 Jun 2025 07:43:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Cotactor-feedack-using-ADC-with-SW-triggering/m-p/2115142#M49837</guid>
      <dc:creator>Joseph_David</dc:creator>
      <dc:date>2025-06-12T07:43:05Z</dc:date>
    </item>
    <item>
      <title>Re: Cotactor feedack using ADC with SW triggering</title>
      <link>https://community.nxp.com/t5/S32K/Cotactor-feedack-using-ADC-with-SW-triggering/m-p/2115643#M49859</link>
      <description>&lt;P&gt;Hi again,&lt;/P&gt;
&lt;P&gt;For ADC SW triggering you could refer directly to RTD examples:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="_Leo__0-1749757713164.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/342756i90B3F580DB682C88/image-size/medium?v=v2&amp;amp;px=400" role="button" title="_Leo__0-1749757713164.png" alt="_Leo__0-1749757713164.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;On the other hand, there is the following community post witch cover more software and hardware triggering methods:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/RTD400-LLD-K344-ADC-SW-HW-trigger/ta-p/1966179" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/RTD400-LLD-K344-ADC-SW-HW-trigger/ta-p/1966179&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I hope this information is helpful.&lt;/P&gt;</description>
      <pubDate>Thu, 12 Jun 2025 19:49:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Cotactor-feedack-using-ADC-with-SW-triggering/m-p/2115643#M49859</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2025-06-12T19:49:07Z</dc:date>
    </item>
  </channel>
</rss>