<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Spi_SetupEB doesn't prepare destination data poiter correctly</title>
    <link>https://community.nxp.com/t5/S32K/Spi-SetupEB-doesn-t-prepare-destination-data-poiter-correctly/m-p/2111257#M49622</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;please search on MBDT Community space directly;&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;There are few threads dealing with this already, for example&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Send-16-Bit-Control-signal-through-SPI/m-p/857355" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Send-16-Bit-Control-signal-through-SPI/m-p/857355&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MR-CANHUBK344-SPI/m-p/1770950" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MR-CANHUBK344-SPI/m-p/1770950&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Or post MBDT/MAtlab/Simulink related question there, so expert can handle it directly.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Thu, 05 Jun 2025 10:23:08 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2025-06-05T10:23:08Z</dc:date>
    <item>
      <title>Spi_SetupEB doesn't prepare destination data poiter correctly</title>
      <link>https://community.nxp.com/t5/S32K/Spi-SetupEB-doesn-t-prepare-destination-data-poiter-correctly/m-p/2110559#M49590</link>
      <description>&lt;P&gt;I'm using&amp;nbsp;S32K3X8EVB-Q289 with MBDT to develop the SPI commnication with FS26.&lt;/P&gt;&lt;P&gt;I've found that if i put the Spi_SetupEB and the Spi_AsyncTransmit into&amp;nbsp; the initialize function of the model the data store memory assigned to Dest Data is always 0 if it's into the inizialize function as well...&lt;/P&gt;&lt;P&gt;If i take the dest Data out with an output port and attach a new data store to it, that data store memory will be filled with the spi data recived.&lt;/P&gt;&lt;P&gt;Why is that possible? Is there a way to solve this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Attached you'll find my project zipped.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jun 2025 15:59:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Spi-SetupEB-doesn-t-prepare-destination-data-poiter-correctly/m-p/2110559#M49590</guid>
      <dc:creator>simon98</dc:creator>
      <dc:date>2025-06-04T15:59:45Z</dc:date>
    </item>
    <item>
      <title>Re: Spi_SetupEB doesn't prepare destination data poiter correctly</title>
      <link>https://community.nxp.com/t5/S32K/Spi-SetupEB-doesn-t-prepare-destination-data-poiter-correctly/m-p/2111257#M49622</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;please search on MBDT Community space directly;&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;There are few threads dealing with this already, for example&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Send-16-Bit-Control-signal-through-SPI/m-p/857355" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Send-16-Bit-Control-signal-through-SPI/m-p/857355&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MR-CANHUBK344-SPI/m-p/1770950" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MR-CANHUBK344-SPI/m-p/1770950&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Or post MBDT/MAtlab/Simulink related question there, so expert can handle it directly.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jun 2025 10:23:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Spi-SetupEB-doesn-t-prepare-destination-data-poiter-correctly/m-p/2111257#M49622</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-06-05T10:23:08Z</dc:date>
    </item>
  </channel>
</rss>