<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: NXPS32K312EVB: SPI - Send uint16 data</title>
    <link>https://community.nxp.com/t5/S32K/NXPS32K312EVB-SPI-Send-uint16-data/m-p/2111255#M49621</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;please search on MBDT Community space directly;&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;There are few threads dealing with this already, for example&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Send-16-Bit-Control-signal-through-SPI/m-p/857355" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Send-16-Bit-Control-signal-through-SPI/m-p/857355&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MR-CANHUBK344-SPI/m-p/1770950" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MR-CANHUBK344-SPI/m-p/1770950&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Or post MBDT/MAtlab/Simulink related question there, so expert can handle it directly.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Thu, 05 Jun 2025 10:21:44 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2025-06-05T10:21:44Z</dc:date>
    <item>
      <title>NXPS32K312EVB: SPI - Send uint16 data</title>
      <link>https://community.nxp.com/t5/S32K/NXPS32K312EVB-SPI-Send-uint16-data/m-p/2110694#M49591</link>
      <description>&lt;P&gt;Team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have an NXP S32K312 EVB and I am using MBDT. I tried flashing an example for SPI (SPI Asynchronous Transfer S32CT) and was able to check the master_send, master_recv on Free Master and confirmed the data transfer.&lt;/P&gt;&lt;P&gt;Now, for the application that I am working on, I have to send 16 bit data to be able to communicate. I used the same example and started to tailor it to my needs and I keep getting errors when trying to build the model saying that the block&amp;nbsp; SPI_SetupEB can only take uint8. I tried to use S32 Config tool and changed the&amp;nbsp;&lt;/P&gt;&lt;P align="left"&gt;SpiChannel_0/SpiDataWidth from 8 to 16 but it is of no help, can you please let me know how I can overcome this issue?&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jun 2025 20:15:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NXPS32K312EVB-SPI-Send-uint16-data/m-p/2110694#M49591</guid>
      <dc:creator>beginner100</dc:creator>
      <dc:date>2025-06-04T20:15:04Z</dc:date>
    </item>
    <item>
      <title>Re: NXPS32K312EVB: SPI - Send uint16 data</title>
      <link>https://community.nxp.com/t5/S32K/NXPS32K312EVB-SPI-Send-uint16-data/m-p/2111255#M49621</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;please search on MBDT Community space directly;&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;There are few threads dealing with this already, for example&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Send-16-Bit-Control-signal-through-SPI/m-p/857355" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Send-16-Bit-Control-signal-through-SPI/m-p/857355&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MR-CANHUBK344-SPI/m-p/1770950" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MR-CANHUBK344-SPI/m-p/1770950&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Or post MBDT/MAtlab/Simulink related question there, so expert can handle it directly.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jun 2025 10:21:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NXPS32K312EVB-SPI-Send-uint16-data/m-p/2111255#M49621</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-06-05T10:21:44Z</dc:date>
    </item>
  </channel>
</rss>