<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: FTM PWM Synchronization：Hardware Trigger</title>
    <link>https://community.nxp.com/t5/S32K/FTM-PWM-Synchronization-Hardware-Trigger/m-p/2109826#M49550</link>
    <description>&lt;P&gt;Thank you for your interest in our products and for contributing to our community.&lt;/P&gt;
&lt;P&gt;Please refer to &lt;EM&gt;4.3.4. Updating FTM registers by hardware trigger—hardware synchronization&lt;/EM&gt; section of &lt;A href="https://www.nxp.com/docs/en/application-note/AN5303.pdf" target="_blank" rel="noopener"&gt;AN5303: Features and Operation Modes of FlexTimer Module on S32K&lt;/A&gt; and to its respective associated file &lt;A href="https://www.nxp.com/webapp/Download?colCode=AN5303SW&amp;amp;location=null" target="_blank" rel="noopener"&gt;AN5303SW&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Test it with the following SW:&lt;BR /&gt;&lt;EM&gt;- S32 Design Studio (S32DS) for ARM 2.2&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- S32 Software Development Kit (SDK) for S32K1xx 3.0.3&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;I hope this information is helpful.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Leonardo&lt;/P&gt;</description>
    <pubDate>Tue, 03 Jun 2025 22:35:18 GMT</pubDate>
    <dc:creator>_Leo_</dc:creator>
    <dc:date>2025-06-03T22:35:18Z</dc:date>
    <item>
      <title>FTM PWM Synchronization：Hardware Trigger</title>
      <link>https://community.nxp.com/t5/S32K/FTM-PWM-Synchronization-Hardware-Trigger/m-p/2109027#M49502</link>
      <description>&lt;P&gt;I am trying to get a better understanding of how the FTM syncronization works using a hardware trigger(TRIG1).&lt;/P&gt;&lt;P&gt;I have already set the SYNCMODE=1, HWTRIGMODE=1, HWWRBUF=1, TRIG1=1 and CNTMAX=1 in FTM0 registers. The FTM0 is in combine mode.&lt;/P&gt;&lt;P&gt;I have also enable the FTM1( Frequency is one-third of FTM0) interrupt to set the SIM_FTMOPT1[FTM1SYNCBIT]=1 and prepare FTM0 CnV register buffer values.&lt;/P&gt;&lt;P&gt;With my understanding, After receiving the FTM1 synchronization signal(SIM_FTMOPT1[FTM1SYNCBIT]=1), FTM0 should update CnV register with the buffer value. However, it does not work according to my expectations and the CnV register does not change.&lt;/P&gt;&lt;P&gt;I am wondering if my understanding of how this works is correct?&lt;/P&gt;&lt;P&gt;How to use the TRIG1(SIM_FTMOPT1[FTM1SYNCBIT]) correctly and When is the sync bit reset to zero?&lt;/P&gt;&lt;P&gt;Thanks for the answer.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jun 2025 02:42:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FTM-PWM-Synchronization-Hardware-Trigger/m-p/2109027#M49502</guid>
      <dc:creator>Scorpio</dc:creator>
      <dc:date>2025-06-03T02:42:18Z</dc:date>
    </item>
    <item>
      <title>Re: FTM PWM Synchronization：Hardware Trigger</title>
      <link>https://community.nxp.com/t5/S32K/FTM-PWM-Synchronization-Hardware-Trigger/m-p/2109826#M49550</link>
      <description>&lt;P&gt;Thank you for your interest in our products and for contributing to our community.&lt;/P&gt;
&lt;P&gt;Please refer to &lt;EM&gt;4.3.4. Updating FTM registers by hardware trigger—hardware synchronization&lt;/EM&gt; section of &lt;A href="https://www.nxp.com/docs/en/application-note/AN5303.pdf" target="_blank" rel="noopener"&gt;AN5303: Features and Operation Modes of FlexTimer Module on S32K&lt;/A&gt; and to its respective associated file &lt;A href="https://www.nxp.com/webapp/Download?colCode=AN5303SW&amp;amp;location=null" target="_blank" rel="noopener"&gt;AN5303SW&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Test it with the following SW:&lt;BR /&gt;&lt;EM&gt;- S32 Design Studio (S32DS) for ARM 2.2&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;- S32 Software Development Kit (SDK) for S32K1xx 3.0.3&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;I hope this information is helpful.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Leonardo&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jun 2025 22:35:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FTM-PWM-Synchronization-Hardware-Trigger/m-p/2109826#M49550</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2025-06-03T22:35:18Z</dc:date>
    </item>
  </channel>
</rss>