<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 FS23 LIN configuration</title>
    <link>https://community.nxp.com/t5/S32K/FS23-LIN-configuration/m-p/2109319#M49519</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I have a setup with S32K1XX MCU and using a FS2303 SBC. I'm trying to enable the LIN communication by setting the M_LIN (0x2B) registry values through SPI&amp;nbsp; (as described in documentation)&lt;/P&gt;&lt;P&gt;Before calling the M_LIN write I'm checking the M_DEV_CFG and the LIN is available ; and the SBS mode is normal .&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've tried to call the the configuration write for M_LIN during INIT phase and also after INIT Mode was closed and the 1st valid watchdog token was sent with the same result.&amp;nbsp;&lt;/P&gt;&lt;P&gt;M_LIN registry value remains 0x0000 (the reset value) and I'm unable to use the communication interface.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 03 Jun 2025 08:34:33 GMT</pubDate>
    <dc:creator>MihaiC</dc:creator>
    <dc:date>2025-06-03T08:34:33Z</dc:date>
    <item>
      <title>FS23 LIN configuration</title>
      <link>https://community.nxp.com/t5/S32K/FS23-LIN-configuration/m-p/2109319#M49519</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I have a setup with S32K1XX MCU and using a FS2303 SBC. I'm trying to enable the LIN communication by setting the M_LIN (0x2B) registry values through SPI&amp;nbsp; (as described in documentation)&lt;/P&gt;&lt;P&gt;Before calling the M_LIN write I'm checking the M_DEV_CFG and the LIN is available ; and the SBS mode is normal .&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've tried to call the the configuration write for M_LIN during INIT phase and also after INIT Mode was closed and the 1st valid watchdog token was sent with the same result.&amp;nbsp;&lt;/P&gt;&lt;P&gt;M_LIN registry value remains 0x0000 (the reset value) and I'm unable to use the communication interface.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jun 2025 08:34:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS23-LIN-configuration/m-p/2109319#M49519</guid>
      <dc:creator>MihaiC</dc:creator>
      <dc:date>2025-06-03T08:34:33Z</dc:date>
    </item>
    <item>
      <title>Re: FS23 LIN configuration</title>
      <link>https://community.nxp.com/t5/S32K/FS23-LIN-configuration/m-p/2109490#M49531</link>
      <description>&lt;P&gt;Hi Mihai,&lt;/P&gt;
&lt;P&gt;I assume you have tried writing 0x4400 to the M_LIN register, right?&lt;/P&gt;
&lt;P&gt;Could you please try writing a different value to see if any write is accepted? Is the PHYG flag set?&lt;/P&gt;
&lt;P&gt;Are you able to use the LIN interface in Debug mode when both CAN and LIN transceivers are set in Active mode by default?&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jun 2025 11:26:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS23-LIN-configuration/m-p/2109490#M49531</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2025-06-03T11:26:00Z</dc:date>
    </item>
    <item>
      <title>Re: FS23 LIN configuration</title>
      <link>https://community.nxp.com/t5/S32K/FS23-LIN-configuration/m-p/2109515#M49535</link>
      <description>&lt;P&gt;Hi Thomas,&lt;/P&gt;&lt;P&gt;I've tried to write 0x4400 , 0x6400, 0x6C00 and some other values with same result - nothing changed.&lt;/P&gt;&lt;P&gt;Writing value through SPI works as the system stays alive while operating using the watchdog mechanism.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The write request reply full reply is :&amp;nbsp;&lt;/P&gt;&lt;P&gt;0x410000E1 - and CRC checks.&amp;nbsp;&lt;/P&gt;&lt;P&gt;From first byte &lt;STRONG&gt;0x41 (0100 0001)&amp;nbsp;&lt;/STRONG&gt;we can determine that&amp;nbsp;&lt;STRONG&gt;SAFETYG is 1&amp;nbsp;&lt;/STRONG&gt;so we have something related with safety , and&amp;nbsp;&lt;STRONG&gt;PHYG is 0.&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;How can I set the SBC to be in debug mode ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you !&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jun 2025 11:56:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS23-LIN-configuration/m-p/2109515#M49535</guid>
      <dc:creator>MihaiC</dc:creator>
      <dc:date>2025-06-03T11:56:38Z</dc:date>
    </item>
    <item>
      <title>Re: FS23 LIN configuration</title>
      <link>https://community.nxp.com/t5/S32K/FS23-LIN-configuration/m-p/2109554#M49538</link>
      <description>&lt;P&gt;Hi Mihai,&lt;/P&gt;
&lt;P&gt;In order to determine why SAFETYG is set, please read the FS_SAFETY_FLG register.&lt;/P&gt;
&lt;P&gt;To enter Debug mode, you need to apply a specific voltage (VDBG_MODE, typ. 4.5V) to the DBG pin during power-up.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jun 2025 13:04:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS23-LIN-configuration/m-p/2109554#M49538</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2025-06-03T13:04:15Z</dc:date>
    </item>
    <item>
      <title>Re: FS23 LIN configuration</title>
      <link>https://community.nxp.com/t5/S32K/FS23-LIN-configuration/m-p/2109561#M49539</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MihaiC_0-1748956094783.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/341124i8F5678B4E7FF675F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="MihaiC_0-1748956094783.png" alt="MihaiC_0-1748956094783.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;MihaiC_0-1748956094783.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;These are the values I'm getting on start up ; Safety flags are 0 but safety output is 0x3800 after boot.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jun 2025 13:10:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS23-LIN-configuration/m-p/2109561#M49539</guid>
      <dc:creator>MihaiC</dc:creator>
      <dc:date>2025-06-03T13:10:52Z</dc:date>
    </item>
    <item>
      <title>Re: FS23 LIN configuration</title>
      <link>https://community.nxp.com/t5/S32K/FS23-LIN-configuration/m-p/2109682#M49547</link>
      <description>&lt;P&gt;Hi Thomas,&lt;/P&gt;&lt;P&gt;some additional information :&amp;nbsp;&lt;/P&gt;&lt;P&gt;for some reason I'm getting the same watchdog token back all the time -&amp;nbsp;0x5AB2&amp;nbsp; in theory I should get 2 different values alternatively.&amp;nbsp;&lt;/P&gt;&lt;P&gt;After asking and replying the current token for 7 times as advised in documentation I'm trying to release both&amp;nbsp;&amp;nbsp;FS0B andLIMP0 by writing required bit array to&amp;nbsp;FS_FS0B_LIMP0_REL (some 1 bit and some parts of current watchdog token). The write also fails with&amp;nbsp; 0x550000&lt;STRONG&gt;FF.&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;My guess is that there is some error that blocks me in enabling the LIN.&lt;/P&gt;&lt;P&gt;At some point we've tried to enable the debug mode by putting some voltage on corresponding pin but for some reason this didn't work as well.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jun 2025 16:35:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS23-LIN-configuration/m-p/2109682#M49547</guid>
      <dc:creator>MihaiC</dc:creator>
      <dc:date>2025-06-03T16:35:45Z</dc:date>
    </item>
  </channel>
</rss>