<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: FS4500 SBC Wdg window change</title>
    <link>https://community.nxp.com/t5/S32K/FS4500-SBC-Wdg-window-change/m-p/2108660#M49483</link>
    <description>&lt;P&gt;Hi&amp;nbsp;Rashiqua,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, you can initialize the FS45 in INIT_FS state with the watchdog window set to 0 (WD_WINDOW_3:0 = 0b0000).&amp;nbsp;Note that this is effective only when the INIT_FS phase is closed, so it requires at least one good watchdog refresh (0x4D when using a default LFSR value of 0xB2) within the 256ms of the INIT_FS timeout.&amp;nbsp;Then you can change the watchdog window duration to a non-zero value in Normal mode.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
    <pubDate>Mon, 02 Jun 2025 13:21:59 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2025-06-02T13:21:59Z</dc:date>
    <item>
      <title>FS4500 SBC Wdg window change</title>
      <link>https://community.nxp.com/t5/S32K/FS4500-SBC-Wdg-window-change/m-p/2108569#M49471</link>
      <description>&lt;P&gt;I wanted to understand if it's possible to initialize the SBC (after LPOFF) with Wdg window selected as 0 in INIT_FS mode. And change the window size to a non-zero window size in 'Normal' mode?Based on the technical reference it appears to be possible to do so but didn't work when I tried this. Can you please suggest how to do this?&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jun 2025 09:44:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS4500-SBC-Wdg-window-change/m-p/2108569#M49471</guid>
      <dc:creator>quadra</dc:creator>
      <dc:date>2025-06-02T09:44:00Z</dc:date>
    </item>
    <item>
      <title>Re: FS4500 SBC Wdg window change</title>
      <link>https://community.nxp.com/t5/S32K/FS4500-SBC-Wdg-window-change/m-p/2108660#M49483</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Rashiqua,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, you can initialize the FS45 in INIT_FS state with the watchdog window set to 0 (WD_WINDOW_3:0 = 0b0000).&amp;nbsp;Note that this is effective only when the INIT_FS phase is closed, so it requires at least one good watchdog refresh (0x4D when using a default LFSR value of 0xB2) within the 256ms of the INIT_FS timeout.&amp;nbsp;Then you can change the watchdog window duration to a non-zero value in Normal mode.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jun 2025 13:21:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS4500-SBC-Wdg-window-change/m-p/2108660#M49483</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2025-06-02T13:21:59Z</dc:date>
    </item>
    <item>
      <title>Re: FS4500 SBC Wdg window change</title>
      <link>https://community.nxp.com/t5/S32K/FS4500-SBC-Wdg-window-change/m-p/2111970#M49658</link>
      <description>Thanks , Tomas. I will try this again.&lt;BR /&gt;Is it correct that a window_size 0 will keep the Wdg disabled? And we can 'enable' it by increasing the window size to non-zero value at 'any time' in Normal mode.</description>
      <pubDate>Fri, 06 Jun 2025 09:19:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS4500-SBC-Wdg-window-change/m-p/2111970#M49658</guid>
      <dc:creator>quadra</dc:creator>
      <dc:date>2025-06-06T09:19:24Z</dc:date>
    </item>
  </channel>
</rss>