<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32K358 Advance the HSE Life Cycle, Debug authorization without source code implementation</title>
    <link>https://community.nxp.com/t5/S32K/S32K358-Advance-the-HSE-Life-Cycle-Debug-authorization-without/m-p/2108463#M49460</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247218"&gt;@HaiHoangSoftware&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It doesn't matter if HSE services are launched by your code running on MCU or by debugger. The result is the same. &lt;/P&gt;
&lt;P&gt;In case of mentioned services, you can take a look at &lt;SPAN&gt;S32K344_CQC_DEMO&lt;/SPAN&gt; in HSE Demo Examples:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;c:\NXP\S32K3_HSE_DemoExamples_1_0_0\S32K3_HSE_DemoExamples\Device_Configuration\S32K344_CQC_DEMO\&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;This demo shows how to set ADKP, how to advance the life cycle etc. &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You can write cmm script to do the same by your debugger - just initialize a service descriptor somewhere in RAM and then launch such service by writing to transmit register in MU. &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Lukas&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 02 Jun 2025 07:05:23 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2025-06-02T07:05:23Z</dc:date>
    <item>
      <title>S32K358 Advance the HSE Life Cycle, Debug authorization without source code implementation</title>
      <link>https://community.nxp.com/t5/S32K/S32K358-Advance-the-HSE-Life-Cycle-Debug-authorization-without/m-p/2108390#M49456</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to test our soft ware in IN_FIELD HSE lifecycle.&lt;/P&gt;&lt;P&gt;The NXP examples shows that the .cmm scripts needs to execute HSE functions from the Demo APP to set HSE attributes for:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Programming/Read ADKP key&lt;/LI&gt;&lt;LI&gt;Change Debug authorization mode to Challenge-Response&lt;/LI&gt;&lt;LI&gt;Authorized Debug&lt;/LI&gt;&lt;LI&gt;Advance HSE Life Cycle&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Is this possible to do all these above tasks without source code implementation?&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jun 2025 02:45:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K358-Advance-the-HSE-Life-Cycle-Debug-authorization-without/m-p/2108390#M49456</guid>
      <dc:creator>HaiHoangSoftware</dc:creator>
      <dc:date>2025-06-02T02:45:48Z</dc:date>
    </item>
    <item>
      <title>Re: S32K358 Advance the HSE Life Cycle, Debug authorization without source code implementation</title>
      <link>https://community.nxp.com/t5/S32K/S32K358-Advance-the-HSE-Life-Cycle-Debug-authorization-without/m-p/2108463#M49460</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247218"&gt;@HaiHoangSoftware&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It doesn't matter if HSE services are launched by your code running on MCU or by debugger. The result is the same. &lt;/P&gt;
&lt;P&gt;In case of mentioned services, you can take a look at &lt;SPAN&gt;S32K344_CQC_DEMO&lt;/SPAN&gt; in HSE Demo Examples:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;c:\NXP\S32K3_HSE_DemoExamples_1_0_0\S32K3_HSE_DemoExamples\Device_Configuration\S32K344_CQC_DEMO\&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;This demo shows how to set ADKP, how to advance the life cycle etc. &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You can write cmm script to do the same by your debugger - just initialize a service descriptor somewhere in RAM and then launch such service by writing to transmit register in MU. &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Lukas&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jun 2025 07:05:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K358-Advance-the-HSE-Life-Cycle-Debug-authorization-without/m-p/2108463#M49460</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2025-06-02T07:05:23Z</dc:date>
    </item>
    <item>
      <title>Re: S32K358 Advance the HSE Life Cycle, Debug authorization without source code implementation</title>
      <link>https://community.nxp.com/t5/S32K/S32K358-Advance-the-HSE-Life-Cycle-Debug-authorization-without/m-p/2108475#M49464</link>
      <description>&lt;P&gt;Yes, the NXP S32Z280-400EVB supports trace functionality using **Arm CoreSight™ technology**, specifically **ETM** for core program tracing. **Lauterbach TRACE32 debuggers are fully compatible** and commonly used for this, enabling detailed analysis. However, directly programming ADKP keys, changing debug authorization modes, or advancing HSE lifecycle states via just `.cmm` scripts is generally **not possible** without corresponding application-level API calls or dedicated tools. NXP and Lauterbach support can provide further guidance on authorized debug and secure provisioning.&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jun 2025 07:21:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K358-Advance-the-HSE-Life-Cycle-Debug-authorization-without/m-p/2108475#M49464</guid>
      <dc:creator>law485</dc:creator>
      <dc:date>2025-06-02T07:21:40Z</dc:date>
    </item>
    <item>
      <title>Re: S32K358 Advance the HSE Life Cycle, Debug authorization without source code implementation</title>
      <link>https://community.nxp.com/t5/S32K/S32K358-Advance-the-HSE-Life-Cycle-Debug-authorization-without/m-p/2109189#M49507</link>
      <description>Thanks for the information</description>
      <pubDate>Tue, 03 Jun 2025 06:33:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K358-Advance-the-HSE-Life-Cycle-Debug-authorization-without/m-p/2109189#M49507</guid>
      <dc:creator>HaiHoangSoftware</dc:creator>
      <dc:date>2025-06-03T06:33:19Z</dc:date>
    </item>
  </channel>
</rss>