<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K116 VLPS mode wake-up on arrival of a CAN message in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K116-VLPS-mode-wake-up-on-arrival-of-a-CAN-message/m-p/2107282#M49368</link>
    <description>&lt;P&gt;PNET feature is CAN FD compatible?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Thu, 29 May 2025 15:28:27 GMT</pubDate>
    <dc:creator>javher4127</dc:creator>
    <dc:date>2025-05-29T15:28:27Z</dc:date>
    <item>
      <title>S32K116 VLPS mode wake-up on arrival of a CAN message</title>
      <link>https://community.nxp.com/t5/S32K/S32K116-VLPS-mode-wake-up-on-arrival-of-a-CAN-message/m-p/2098923#M48912</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I would like to know if it is possible with the S32K116 microcontroller to wake up from VLPS power mode with the arrival of CAN messages.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 16 May 2025 10:02:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K116-VLPS-mode-wake-up-on-arrival-of-a-CAN-message/m-p/2098923#M48912</guid>
      <dc:creator>javher4127</dc:creator>
      <dc:date>2025-05-16T10:02:13Z</dc:date>
    </item>
    <item>
      <title>Re: S32K116 VLPS mode wake-up on arrival of a CAN message</title>
      <link>https://community.nxp.com/t5/S32K/S32K116-VLPS-mode-wake-up-on-arrival-of-a-CAN-message/m-p/2099107#M48930</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/250557"&gt;@javher4127&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;For S32K1 devices, self-wakeup from CAN module is not supported in VLPS mode. You can see that CAN module is OFF in&amp;nbsp;&lt;STRONG&gt;Table 39-4.&lt;/STRONG&gt;&amp;nbsp;(Module operation in available power modes) from &lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K1XXRM" target="_self"&gt;S32K-RM&lt;/A&gt;.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt; PNET features is used to wake up from STOP1/STOP2 modes in those instances where PNET is included, but this does not apply for VLPS mode. As a workaround, you can use any other pin (or even the same CAN_RX pin changing PORT configuration) to generate an interrupt when MCU is on VLPS mode. This can wake the CPU and then restore activity on CAN module.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 16 May 2025 16:31:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K116-VLPS-mode-wake-up-on-arrival-of-a-CAN-message/m-p/2099107#M48930</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-05-16T16:31:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32K116 VLPS mode wake-up on arrival of a CAN message</title>
      <link>https://community.nxp.com/t5/S32K/S32K116-VLPS-mode-wake-up-on-arrival-of-a-CAN-message/m-p/2107282#M49368</link>
      <description>&lt;P&gt;PNET feature is CAN FD compatible?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 29 May 2025 15:28:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K116-VLPS-mode-wake-up-on-arrival-of-a-CAN-message/m-p/2107282#M49368</guid>
      <dc:creator>javher4127</dc:creator>
      <dc:date>2025-05-29T15:28:27Z</dc:date>
    </item>
    <item>
      <title>Re: S32K116 VLPS mode wake-up on arrival of a CAN message</title>
      <link>https://community.nxp.com/t5/S32K/S32K116-VLPS-mode-wake-up-on-arrival-of-a-CAN-message/m-p/2107291#M49369</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/250557"&gt;@javher4127&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;No, wakeup functionality is not available for messages in CAN FD format. When in Pretended Networking mode, CAN FD format messages are ignored.&lt;/P&gt;</description>
      <pubDate>Thu, 29 May 2025 15:46:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K116-VLPS-mode-wake-up-on-arrival-of-a-CAN-message/m-p/2107291#M49369</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-05-29T15:46:39Z</dc:date>
    </item>
  </channel>
</rss>