<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144 IAP implementation in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-IAP-implementation/m-p/929791#M4928</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no example code directly for the S32K144, however, it can be migrated to S32K144.&lt;/P&gt;&lt;P&gt;I have not migrated this example code from S32K148 to S32K144, but below points should be considered:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;There are differences in the memory address range. Please refer to S32K1xx_Memory_Map.xlsx document attached to the RM rev 9.&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Sector size of 2 KB for non-interleaved configurations (i.e., 256 KB and less). 4 KB for interleaved configurations (512 KB and greater)&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;S32K144:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;The 512KB FTFC flash module consists of two NVM read partitions and one FlexRAM&lt;BR /&gt;block:&lt;BR /&gt;• One 512KB program flash read partition (interleaved 2 × 256KB)&lt;BR /&gt;• One 64KB FlexNVM read partition (&lt;STRONG&gt;non-interleaved&lt;/STRONG&gt; 1 × 64KB)&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Jun 2019 10:54:56 GMT</pubDate>
    <dc:creator>dianabatrlova</dc:creator>
    <dc:date>2019-06-18T10:54:56Z</dc:date>
    <item>
      <title>S32K144 IAP implementation</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-IAP-implementation/m-p/929787#M4924</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there an example shows how to implement the IAP with S32K144 use &lt;STRONG&gt;S32DS&lt;/STRONG&gt;?&lt;/P&gt;&lt;P&gt;1. how to implement the bootloader code, where to set the app address, how to jump to app&lt;/P&gt;&lt;P&gt;2. how to implement the app code, how to flash the app code&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My goal is to update the app code via the can bus, and my first step is to implement the IAP via serial port.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jun 2019 02:50:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-IAP-implementation/m-p/929787#M4924</guid>
      <dc:creator>jay_zhang</dc:creator>
      <dc:date>2019-06-17T02:50:16Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 IAP implementation</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-IAP-implementation/m-p/929788#M4925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Anybody can help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jun 2019 02:59:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-IAP-implementation/m-p/929788#M4925</guid>
      <dc:creator>jay_zhang</dc:creator>
      <dc:date>2019-06-17T02:59:35Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 IAP implementation</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-IAP-implementation/m-p/929789#M4926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Zhang,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to recommend application note AN12218 for the serial S32K1xx Bootloader&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12218.pdf" title="https://www.nxp.com/docs/en/application-note/AN12218.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12218.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;SW:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note-software/AN12218SW.zip" title="https://www.nxp.com/docs/en/application-note-software/AN12218SW.zip"&gt;https://www.nxp.com/docs/en/application-note-software/AN12218SW.zip&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I believe the document and software answer your questions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, we have no official example project for the CAN bootloader, however, you can modify the AN12218 to use CAN interface.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jun 2019 07:30:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-IAP-implementation/m-p/929789#M4926</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2019-06-17T07:30:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 IAP implementation</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-IAP-implementation/m-p/929790#M4927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Batriova,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your information, I think it is useful to me.&lt;/P&gt;&lt;P&gt;I find the example code is based on S32K148, is there a version that is S32K144?&lt;/P&gt;&lt;P&gt;If not, can you tell me which code needs to modify?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jun 2019 08:41:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-IAP-implementation/m-p/929790#M4927</guid>
      <dc:creator>jay_zhang</dc:creator>
      <dc:date>2019-06-17T08:41:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 IAP implementation</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-IAP-implementation/m-p/929791#M4928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no example code directly for the S32K144, however, it can be migrated to S32K144.&lt;/P&gt;&lt;P&gt;I have not migrated this example code from S32K148 to S32K144, but below points should be considered:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;There are differences in the memory address range. Please refer to S32K1xx_Memory_Map.xlsx document attached to the RM rev 9.&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Sector size of 2 KB for non-interleaved configurations (i.e., 256 KB and less). 4 KB for interleaved configurations (512 KB and greater)&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;S32K144:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;The 512KB FTFC flash module consists of two NVM read partitions and one FlexRAM&lt;BR /&gt;block:&lt;BR /&gt;• One 512KB program flash read partition (interleaved 2 × 256KB)&lt;BR /&gt;• One 64KB FlexNVM read partition (&lt;STRONG&gt;non-interleaved&lt;/STRONG&gt; 1 × 64KB)&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jun 2019 10:54:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-IAP-implementation/m-p/929791#M4928</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2019-06-18T10:54:56Z</dc:date>
    </item>
  </channel>
</rss>