<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックFS26 driver Autocore compatibility issue?</title>
    <link>https://community.nxp.com/t5/S32K/FS26-driver-Autocore-compatibility-issue/m-p/2100652#M49011</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to integrate the FS26 SBC device driver into a project with Autocore. The problem is that que Wdg_43_fs26 module is not loaded by the tresos so it is not available to be added to the project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried both, the normal installation with the plugins linked to the tresos installation and the manual copy of both the&amp;nbsp; Sbc_fs26_TS_T40D34M40I0R0 and&amp;nbsp;Wdg_43_fs26_TS_T40D34M40I0R0 folders into the Tresos plugins folder, but the result is the same in both cases.&lt;/P&gt;&lt;P&gt;The thing is that the&amp;nbsp;Sbc_fs26 module is correctly loaded into the tresos module list, but the Wdg_43_fs26 does not appear in the module list no matter what.&lt;/P&gt;&lt;P&gt;Is there any kind of compatibility issue between the Autocore and this Wdg driver?&lt;/P&gt;&lt;P&gt;I have attached an image related with the issue. The MCU is the S32K344. The module and SW versions are the following ones:&lt;/P&gt;&lt;P&gt;EB Tresos 29.3.0&lt;/P&gt;&lt;P&gt;Autocore OS 6.1&lt;/P&gt;&lt;P&gt;SBC Driver:&amp;nbsp;S32K3xx_SBC_FS26_R21-11_4.0.0&lt;/P&gt;&lt;P&gt;RTD Driver:&amp;nbsp;SW32K3_S32M27x_RTD_R21-11_4.0.0_P19&lt;/P&gt;&lt;P&gt;Any help will be appreciated, thanks in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 20 May 2025 11:49:47 GMT</pubDate>
    <dc:creator>Oliver91</dc:creator>
    <dc:date>2025-05-20T11:49:47Z</dc:date>
    <item>
      <title>FS26 driver Autocore compatibility issue?</title>
      <link>https://community.nxp.com/t5/S32K/FS26-driver-Autocore-compatibility-issue/m-p/2100652#M49011</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to integrate the FS26 SBC device driver into a project with Autocore. The problem is that que Wdg_43_fs26 module is not loaded by the tresos so it is not available to be added to the project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried both, the normal installation with the plugins linked to the tresos installation and the manual copy of both the&amp;nbsp; Sbc_fs26_TS_T40D34M40I0R0 and&amp;nbsp;Wdg_43_fs26_TS_T40D34M40I0R0 folders into the Tresos plugins folder, but the result is the same in both cases.&lt;/P&gt;&lt;P&gt;The thing is that the&amp;nbsp;Sbc_fs26 module is correctly loaded into the tresos module list, but the Wdg_43_fs26 does not appear in the module list no matter what.&lt;/P&gt;&lt;P&gt;Is there any kind of compatibility issue between the Autocore and this Wdg driver?&lt;/P&gt;&lt;P&gt;I have attached an image related with the issue. The MCU is the S32K344. The module and SW versions are the following ones:&lt;/P&gt;&lt;P&gt;EB Tresos 29.3.0&lt;/P&gt;&lt;P&gt;Autocore OS 6.1&lt;/P&gt;&lt;P&gt;SBC Driver:&amp;nbsp;S32K3xx_SBC_FS26_R21-11_4.0.0&lt;/P&gt;&lt;P&gt;RTD Driver:&amp;nbsp;SW32K3_S32M27x_RTD_R21-11_4.0.0_P19&lt;/P&gt;&lt;P&gt;Any help will be appreciated, thanks in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 May 2025 11:49:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS26-driver-Autocore-compatibility-issue/m-p/2100652#M49011</guid>
      <dc:creator>Oliver91</dc:creator>
      <dc:date>2025-05-20T11:49:47Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 driver Autocore compatibility issue?</title>
      <link>https://community.nxp.com/t5/S32K/FS26-driver-Autocore-compatibility-issue/m-p/2100672#M49012</link>
      <description>Sorry, the RTD driver is the SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311, which I think is included with this Autocore release (Autocore 8.8.9 in the NXP download page)</description>
      <pubDate>Tue, 20 May 2025 12:09:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS26-driver-Autocore-compatibility-issue/m-p/2100672#M49012</guid>
      <dc:creator>Oliver91</dc:creator>
      <dc:date>2025-05-20T12:09:37Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 driver Autocore compatibility issue?</title>
      <link>https://community.nxp.com/t5/S32K/FS26-driver-Autocore-compatibility-issue/m-p/2101258#M49032</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220202"&gt;@quangvuanh&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you please help with this issue regarding the FS26 driver?&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; BRs, Tomas&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 21 May 2025 06:44:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS26-driver-Autocore-compatibility-issue/m-p/2101258#M49032</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2025-05-21T06:44:08Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 driver Autocore compatibility issue?</title>
      <link>https://community.nxp.com/t5/S32K/FS26-driver-Autocore-compatibility-issue/m-p/2111060#M49609</link>
      <description>&lt;P&gt;Shall I assume this is a bug?&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jun 2025 07:36:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS26-driver-Autocore-compatibility-issue/m-p/2111060#M49609</guid>
      <dc:creator>Oliver91</dc:creator>
      <dc:date>2025-06-05T07:36:17Z</dc:date>
    </item>
  </channel>
</rss>