<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックSPI Driver using for S32K311NHT0MLFST</title>
    <link>https://community.nxp.com/t5/S32K/SPI-Driver-using-for-S32K311NHT0MLFST/m-p/2100422#M48980</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;&lt;SPAN&gt;S32K311NHT0MLFST for my project.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I am trying to configure the SPI driver. Is there any example code available for the particular controller or a controller from the same family.&lt;/P&gt;</description>
    <pubDate>Tue, 20 May 2025 07:04:06 GMT</pubDate>
    <dc:creator>rahupat</dc:creator>
    <dc:date>2025-05-20T07:04:06Z</dc:date>
    <item>
      <title>SPI Driver using for S32K311NHT0MLFST</title>
      <link>https://community.nxp.com/t5/S32K/SPI-Driver-using-for-S32K311NHT0MLFST/m-p/2100422#M48980</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;&lt;SPAN&gt;S32K311NHT0MLFST for my project.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I am trying to configure the SPI driver. Is there any example code available for the particular controller or a controller from the same family.&lt;/P&gt;</description>
      <pubDate>Tue, 20 May 2025 07:04:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SPI-Driver-using-for-S32K311NHT0MLFST/m-p/2100422#M48980</guid>
      <dc:creator>rahupat</dc:creator>
      <dc:date>2025-05-20T07:04:06Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Driver using for S32K311NHT0MLFST</title>
      <link>https://community.nxp.com/t5/S32K/SPI-Driver-using-for-S32K311NHT0MLFST/m-p/2101144#M49026</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;As you know, S32K3 has many derivatives, so to reduce effort, in the most recent RTD releases we only provide examples for K344, K358, K388 and K396. Examples of other derivatives can be created based on these existing examples.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Do you use AUTOSAR MCAL?&lt;BR /&gt;I happen to have S32K311 SPI example based on MCAL. One is for RTD4.0.0 and the other is for RTD3.0.0 combined with FS23.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 21 May 2025 04:08:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SPI-Driver-using-for-S32K311NHT0MLFST/m-p/2101144#M49026</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-05-21T04:08:54Z</dc:date>
    </item>
  </channel>
</rss>