<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K3xx SPI debug in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K3xx-SPI-debug/m-p/2099610#M48945</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;While debugging the SPI example code without a breakpoint, the program enters the startup code. Why does this happen? Is there any issue, and how can it be resolved?&lt;/P&gt;&lt;P&gt;/*BKPT #1 - removed to avoid debug fault being escalated to hardfault when debugger is not attached or on VDK*/&lt;BR /&gt;/* last instruction for the debugger to dump results data */&lt;BR /&gt;.globl _end_of_eunit_test&lt;BR /&gt;_end_of_eunit_test:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Karmegan C&lt;/P&gt;</description>
    <pubDate>Mon, 19 May 2025 07:45:14 GMT</pubDate>
    <dc:creator>karmegancjk</dc:creator>
    <dc:date>2025-05-19T07:45:14Z</dc:date>
    <item>
      <title>S32K3xx SPI debug</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-SPI-debug/m-p/2099610#M48945</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;While debugging the SPI example code without a breakpoint, the program enters the startup code. Why does this happen? Is there any issue, and how can it be resolved?&lt;/P&gt;&lt;P&gt;/*BKPT #1 - removed to avoid debug fault being escalated to hardfault when debugger is not attached or on VDK*/&lt;BR /&gt;/* last instruction for the debugger to dump results data */&lt;BR /&gt;.globl _end_of_eunit_test&lt;BR /&gt;_end_of_eunit_test:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Karmegan C&lt;/P&gt;</description>
      <pubDate>Mon, 19 May 2025 07:45:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-SPI-debug/m-p/2099610#M48945</guid>
      <dc:creator>karmegancjk</dc:creator>
      <dc:date>2025-05-19T07:45:14Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3xx SPI debug</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-SPI-debug/m-p/2102918#M49104</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241477"&gt;@karmegancjk&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I see you are using an example from the RTD package, which S32DS &amp;amp; RTD version are you using? And which example are you running?&lt;/P&gt;
&lt;P&gt;I tested &lt;STRONG&gt;Lpspi_Ip_HalfDuplexTransfer_S32K344&lt;/STRONG&gt; and it works as expected:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_0-1747938459019.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/339293i325E4619B10EF0DD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_0-1747938459019.png" alt="Julin_AragnM_0-1747938459019.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Also, could you share more information on what you mean by "&lt;SPAN&gt;While debugging the SPI example code without a breakpoint"? Are you disabling the breakpoint at main when connecting with the debugger?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 22 May 2025 18:28:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-SPI-debug/m-p/2102918#M49104</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-05-22T18:28:41Z</dc:date>
    </item>
  </channel>
</rss>