<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: Unified Bootloader Demo error CANTP_AbortTxMsg</title>
    <link>https://community.nxp.com/t5/S32K/Unified-Bootloader-Demo-error-CANTP-AbortTxMsg/m-p/2095291#M48648</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P class="DoNormal"&gt;I’m sorry to say that Unified bootloader shared on the community is only unofficial demo provided AS IS with no guarantees and no support. Currently we do not have resources to support this demo. We apologize for any inconvenience.&lt;/P&gt;
&lt;P class="DoNormal"&gt;Just simple note for FlexCAN setting, do not use FIRC as CAN protocol clock, rather select external crystal or PLL.&lt;/P&gt;
&lt;P class="DoNormal"&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Mon, 12 May 2025 08:04:58 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2025-05-12T08:04:58Z</dc:date>
    <item>
      <title>Unified Bootloader Demo error CANTP_AbortTxMsg</title>
      <link>https://community.nxp.com/t5/S32K/Unified-Bootloader-Demo-error-CANTP-AbortTxMsg/m-p/2094891#M48624</link>
      <description>&lt;P&gt;Hi&lt;BR /&gt;&lt;BR /&gt;I am working on &lt;STRONG&gt;UBL V2.1&lt;/STRONG&gt; and using &lt;STRONG&gt;S32K312EVB-Q172 board&lt;/STRONG&gt;. My current &lt;STRONG&gt;S32 DS version 3.4&lt;/STRONG&gt; and the RTD is&amp;nbsp;&lt;STRONG&gt;PlatformSDK_S32K3_2022_03_S32K312_M7 Version 2.0.0&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;I am using project source code provided here :&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099&lt;/A&gt;&lt;BR /&gt;with EcuBus-Pro software.&lt;BR /&gt;&lt;BR /&gt;When UDS command was sent, I could receive it correctly (e.g. UDS_DigSession). But while responding back to Tester (EcuBus-Pro), Its failing.&lt;BR /&gt;&lt;BR /&gt;I am getting error msg in Terminal;&lt;/P&gt;&lt;P&gt;"CANTP_AbortTxMsg&lt;/P&gt;&lt;P&gt;TX msg failed callback=0, status=2"&lt;BR /&gt;&lt;BR /&gt;When I traced the code, I found that&amp;nbsp;&lt;BR /&gt;SendMsg()--&amp;gt;TP_DriverReadDataFromTP()---&amp;gt;CANTP_DriverReadDataFromCANTP() returning FALSE. I have attached all the related pics for reference. Please go through them.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Note: I have replaced the binaries present in bin folder of EcuBus-Pro Project, with the S32K312 binaries. Made changed in EcuBus Script accordingly. Its screenshot is also attached.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Need support for resolving this issue.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thank You.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 10 May 2025 09:46:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unified-Bootloader-Demo-error-CANTP-AbortTxMsg/m-p/2094891#M48624</guid>
      <dc:creator>Dnyan</dc:creator>
      <dc:date>2025-05-10T09:46:47Z</dc:date>
    </item>
    <item>
      <title>Re: Unified Bootloader Demo error CANTP_AbortTxMsg</title>
      <link>https://community.nxp.com/t5/S32K/Unified-Bootloader-Demo-error-CANTP-AbortTxMsg/m-p/2095291#M48648</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P class="DoNormal"&gt;I’m sorry to say that Unified bootloader shared on the community is only unofficial demo provided AS IS with no guarantees and no support. Currently we do not have resources to support this demo. We apologize for any inconvenience.&lt;/P&gt;
&lt;P class="DoNormal"&gt;Just simple note for FlexCAN setting, do not use FIRC as CAN protocol clock, rather select external crystal or PLL.&lt;/P&gt;
&lt;P class="DoNormal"&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 12 May 2025 08:04:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unified-Bootloader-Demo-error-CANTP-AbortTxMsg/m-p/2095291#M48648</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-05-12T08:04:58Z</dc:date>
    </item>
    <item>
      <title>Re: Unified Bootloader Demo error CANTP_AbortTxMsg</title>
      <link>https://community.nxp.com/t5/S32K/Unified-Bootloader-Demo-error-CANTP-AbortTxMsg/m-p/2096498#M48722</link>
      <description>&lt;P&gt;Thanks again for your previous response.&lt;BR /&gt;&lt;BR /&gt;Since the UBL project I’m using is an unofficial demo, I understand it may contain limitations or bugs. To avoid starting completely from scratch, I wanted to ask if NXP provides any &lt;STRONG&gt;official or recommended reference bootloader project&lt;/STRONG&gt;—either for the S32K3xx series or for any other NXP MCU that I can refer to and adapt for my target (S32K312/324/344).&lt;/P&gt;&lt;P&gt;Even if not specifically for the S32K312, having access to &lt;STRONG&gt;an official bootloader source&lt;/STRONG&gt; (&lt;STRONG&gt;or link to such resources or documentation&lt;/STRONG&gt;) for &lt;STRONG&gt;any supported platform&lt;/STRONG&gt; would be a huge help. I can use that as a reliable reference and adapt it to my target device.&lt;/P&gt;&lt;P&gt;Your support will truly help move this forward, and I hope some guidance or reference can be provided.&lt;/P&gt;</description>
      <pubDate>Tue, 13 May 2025 12:28:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unified-Bootloader-Demo-error-CANTP-AbortTxMsg/m-p/2096498#M48722</guid>
      <dc:creator>Dnyan</dc:creator>
      <dc:date>2025-05-13T12:28:13Z</dc:date>
    </item>
    <item>
      <title>Re: Unified Bootloader Demo error CANTP_AbortTxMsg</title>
      <link>https://community.nxp.com/t5/S32K/Unified-Bootloader-Demo-error-CANTP-AbortTxMsg/m-p/2098022#M48828</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;you can refer to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32K3-Firmware-Update/td-p/2090573" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K3-Firmware-Update/td-p/2090573&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 15 May 2025 09:34:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unified-Bootloader-Demo-error-CANTP-AbortTxMsg/m-p/2098022#M48828</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-05-15T09:34:52Z</dc:date>
    </item>
  </channel>
</rss>