<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K344 Makefile/FreeRTOS project in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-Makefile-FreeRTOS-project/m-p/2094925#M48628</link>
    <description>&lt;P&gt;We are interested in using S32K344 and purchased a&amp;nbsp;&lt;SPAN&gt;S32K344-WB devel board.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Since our developers are mostly familiar with non-automotive ARM processors the roadmap includes FreeRTOS with SafeRTOS port once the prototype is working.&lt;BR /&gt;We want to use:&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN&gt;C++17&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Makefile/cmake build env running on Linux&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;FreeRTOS&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;arm-none-eabi toolchain&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN&gt;I understand that any HAL/drivers will need to be written from scratch (we DONT want to use anything Autosar)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there any sample project available that checks some of those boxes? Basic makefile project with working linker script and startup would be immensely helpful in getting started quickly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 11 May 2025 19:33:05 GMT</pubDate>
    <dc:creator>segfaulty</dc:creator>
    <dc:date>2025-05-11T19:33:05Z</dc:date>
    <item>
      <title>S32K344 Makefile/FreeRTOS project</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Makefile-FreeRTOS-project/m-p/2094925#M48628</link>
      <description>&lt;P&gt;We are interested in using S32K344 and purchased a&amp;nbsp;&lt;SPAN&gt;S32K344-WB devel board.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Since our developers are mostly familiar with non-automotive ARM processors the roadmap includes FreeRTOS with SafeRTOS port once the prototype is working.&lt;BR /&gt;We want to use:&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN&gt;C++17&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Makefile/cmake build env running on Linux&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;FreeRTOS&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;arm-none-eabi toolchain&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN&gt;I understand that any HAL/drivers will need to be written from scratch (we DONT want to use anything Autosar)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there any sample project available that checks some of those boxes? Basic makefile project with working linker script and startup would be immensely helpful in getting started quickly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 11 May 2025 19:33:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Makefile-FreeRTOS-project/m-p/2094925#M48628</guid>
      <dc:creator>segfaulty</dc:creator>
      <dc:date>2025-05-11T19:33:05Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 Makefile/FreeRTOS project</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Makefile-FreeRTOS-project/m-p/2096504#M48723</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/232381"&gt;@segfaulty&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;NXP provides only FreeRTOS driver that is an extension to the S32K3xx RTD drivers, which has also low-level IP drivers that are not Autosar compatible.&lt;/P&gt;
&lt;P&gt;The driver is included in the S32K3xx reference software.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D" target="_blank"&gt;https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Unfortunately, there is no example of such a makefile.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 May 2025 12:34:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Makefile-FreeRTOS-project/m-p/2096504#M48723</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-05-13T12:34:24Z</dc:date>
    </item>
  </channel>
</rss>